Throughput Test helper#

Helper for throughput tests

Modules#

allowlist_s

throughput_t

Enumerations#

enum
act_none = 0
act_discover_service
act_discover_characteristics
act_enable_transmission_notification
act_enable_notification
act_enable_indication
act_subscribe_result
}
enum
THROUGHPUT_ROLE_PERIPHERAL
THROUGHPUT_ROLE_CENTRAL
}

Role enum type.

enum
THROUGHPUT_STATE_UNINITALIZED
THROUGHPUT_STATE_DISCONNECTED
THROUGHPUT_STATE_CONNECTED
THROUGHPUT_STATE_SUBSCRIBED
THROUGHPUT_STATE_TEST
THROUGHPUT_STATE_TEST_FINISH
THROUGHPUT_STATE_UNINITALIZING
}

State enum type.

enum
THROUGHPUT_MODE_CONTINUOUS
THROUGHPUT_MODE_FIXED_TIME
THROUGHPUT_MODE_FIXED_LENGTH
}

Mode enum type.

enum
THROUGHPUT_DISCOVERY_STATE_IDLE
THROUGHPUT_DISCOVERY_STATE_CONN
THROUGHPUT_DISCOVERY_STATE_SCAN
THROUGHPUT_DISCOVERY_STATE_SERVICE
THROUGHPUT_DISCOVERY_STATE_CHARACTERISTICS
THROUGHPUT_DISCOVERY_STATE_FINISHED
}

Discovery state.

Typedefs#

typedef int8_t

TX power type.

typedef int8_t
typedef uint16_t

PDU size type.

typedef uint16_t

MTU size type.

typedef uint16_t

Data size type.

typedef sl_bt_gap_phy_coding_t
typedef sl_bt_scanner_scan_phy_t
typedef sl_bt_gatt_client_config_flag_t

Notification/indication type.

typedef uint32_t

Throughput type.

typedef uint32_t

Data counter type type.

typedef uint32_t

Time type type.

typedef struct allowlist_s

Throughput test allowlist structure.

Macros#

#define

The default PDU size if 27 bytes according to the Core Specification.

#define
THROUGHPUT_MAXIMUM_MTU_SIZE (SL_BGAPI_MAX_PAYLOAD_SIZE - 7)

The maximum available MTU size.

#define
#define
CLI_OK "OK" APP_LOG_NEW_LINE
#define
CLI_ERROR "ERROR" APP_LOG_NEW_LINE

Enumeration Documentation#

action_t#

action_t

Discovering services/characteristics and subscribing raises procedure_complete events Actions are used to indicate which procedure was completed.

Enumerator
act_none
act_discover_service
act_discover_characteristics
act_enable_transmission_notification
act_enable_notification
act_enable_indication
act_subscribe_result

throughput_role_t#

throughput_role_t

Role enum type.

Enumerator
THROUGHPUT_ROLE_PERIPHERAL
THROUGHPUT_ROLE_CENTRAL

throughput_state_t#

throughput_state_t

State enum type.

Enumerator
THROUGHPUT_STATE_UNINITALIZED
THROUGHPUT_STATE_DISCONNECTED
THROUGHPUT_STATE_CONNECTED
THROUGHPUT_STATE_SUBSCRIBED
THROUGHPUT_STATE_TEST
THROUGHPUT_STATE_TEST_FINISH
THROUGHPUT_STATE_UNINITALIZING

throughput_mode_t#

throughput_mode_t

Mode enum type.

Enumerator
THROUGHPUT_MODE_CONTINUOUS
THROUGHPUT_MODE_FIXED_TIME
THROUGHPUT_MODE_FIXED_LENGTH

throughput_discovery_state_t#

throughput_discovery_state_t

Discovery state.

Enumerator
THROUGHPUT_DISCOVERY_STATE_IDLE
THROUGHPUT_DISCOVERY_STATE_CONN
THROUGHPUT_DISCOVERY_STATE_SCAN
THROUGHPUT_DISCOVERY_STATE_SERVICE
THROUGHPUT_DISCOVERY_STATE_CHARACTERISTICS
THROUGHPUT_DISCOVERY_STATE_FINISHED

Typedef Documentation#

throughput_tx_power_t#

typedef int8_t throughput_tx_power_t

TX power type.


throughput_rssi_t#

typedef int8_t throughput_rssi_t

RSSI type.


throughput_pdu_size_t#

typedef uint16_t throughput_pdu_size_t

PDU size type.


throughput_mtu_size_t#

typedef uint16_t throughput_mtu_size_t

MTU size type.


throughput_data_size_t#

typedef uint16_t throughput_data_size_t

Data size type.


throughput_phy_t#

typedef sl_bt_gap_phy_coding_t throughput_phy_t

PHY type.


throughput_scan_phy_t#

typedef sl_bt_scanner_scan_phy_t throughput_scan_phy_t

throughput_notification_t#

typedef sl_bt_gatt_client_config_flag_t throughput_notification_t

Notification/indication type.


throughput_value_t#

typedef uint32_t throughput_value_t

Throughput type.


throughput_count_t#

typedef uint32_t throughput_count_t

Data counter type type.


throughput_time_t#

typedef uint32_t throughput_time_t

Time type type.


throughput_allowlist_t#

typedef struct allowlist_s throughput_allowlist_t

Throughput test allowlist structure.


Macro Definition Documentation#

THROUGHPUT_DEFAULT_PDU_SIZE#

#define THROUGHPUT_DEFAULT_PDU_SIZE
Value:
27u

The default PDU size if 27 bytes according to the Core Specification.


THROUGHPUT_MAXIMUM_MTU_SIZE#

#define THROUGHPUT_MAXIMUM_MTU_SIZE
Value:
(SL_BGAPI_MAX_PAYLOAD_SIZE - 7)

The maximum available MTU size.


CLI_RESPONSE#

#define CLI_RESPONSE
Value:
(...)

CLI_OK#

#define CLI_OK
Value:
"OK" APP_LOG_NEW_LINE

CLI_ERROR#

#define CLI_ERROR
Value:
"ERROR" APP_LOG_NEW_LINE