Scanner#

Scanner.

The commands and events in this class provides scanning functionality. There are functionality differences depending on included components:

The bluetooth_feature_legacy_scanner component is included but the bluetooth_feature_extended_scanner is not:

The bluetooth_feature_extended_scanner component is included:

Modules#

Event Type Flags of Advertisement Reports

Option Flags to Specify Scanning Options

sl_bt_evt_scanner_legacy_advertisement_report

sl_bt_evt_scanner_extended_advertisement_report

Enumerations#

enum
sl_bt_scanner_discover_limited = 0x0
sl_bt_scanner_discover_generic = 0x1
sl_bt_scanner_discover_observation = 0x2
}

These values indicate which Bluetooth discovery mode to use when scanning for advertising devices.

enum
sl_bt_scanner_scan_mode_passive = 0x0
sl_bt_scanner_scan_mode_active = 0x1
}

The scanning modes.

enum
sl_bt_scanner_scan_phy_1m = 0x1
sl_bt_scanner_scan_phy_coded = 0x4
sl_bt_scanner_scan_phy_1m_and_coded = 0x5
}

The enum defines the scanning PHYs.

enum
sl_bt_scanner_data_status_complete = 0x0
sl_bt_scanner_data_status_incomplete_more = 0x1
sl_bt_scanner_data_status_incomplete_nomore = 0x2
}

Defines the data completeness status types of an advertisement reported by the scanner.

enum
sl_bt_scanner_filter_policy_basic_unfiltered = 0x0
sl_bt_scanner_filter_policy_basic_filtered = 0x1
sl_bt_scanner_filter_policy_extended_unfiltered = 0x2
sl_bt_scanner_filter_policy_extended_filtered = 0x3
}

The scanning filter policy setting determines which advertisements and scan responses are delivered to the application when scanning. See the Bluetooth Core specification Volume 6, Part B, Section 4.3.3 "Scanning filter policy" for a detailed description of this setting.

Functions#

sl_status_t
sl_bt_scanner_set_parameters(uint8_t mode, uint16_t interval, uint16_t window)
sl_status_t
sl_bt_scanner_set_parameters_and_filter(uint8_t mode, uint16_t interval, uint16_t window, uint32_t flags, uint8_t filter_policy)
sl_status_t
sl_bt_scanner_start(uint8_t scanning_phy, uint8_t discover_mode)
sl_status_t

Enumeration Documentation#

sl_bt_scanner_discover_mode_t#

sl_bt_scanner_discover_mode_t

These values indicate which Bluetooth discovery mode to use when scanning for advertising devices.

Enumerator
sl_bt_scanner_discover_limited

(0x0) Discover only limited discoverable devices.

sl_bt_scanner_discover_generic

(0x1) Discover limited and general discoverable devices.

sl_bt_scanner_discover_observation

(0x2) Discover non-discoverable, limited and general discoverable devices.


sl_bt_scanner_scan_mode_t#

sl_bt_scanner_scan_mode_t

The scanning modes.

Enumerator
sl_bt_scanner_scan_mode_passive

(0x0) Passive scanning mode where the device only listens to advertising packets and does not transmit packets

sl_bt_scanner_scan_mode_active

(0x1) Active scanning mode where the device sends out a scan request packet upon receiving a scannable advertising packet from a remote device and listens to the scan response packet from the remote device


sl_bt_scanner_scan_phy_t#

sl_bt_scanner_scan_phy_t

The enum defines the scanning PHYs.

Enumerator
sl_bt_scanner_scan_phy_1m

(0x1) Initiate the scanning on the 1M PHY

sl_bt_scanner_scan_phy_coded

(0x4) Initiate the scanning on the Coded PHY

sl_bt_scanner_scan_phy_1m_and_coded

(0x5) Simultaneous scanning by initiating the scanning on the 1M and Coded PHY alternatively


sl_bt_scanner_data_status_t#

sl_bt_scanner_data_status_t

Defines the data completeness status types of an advertisement reported by the scanner.

Enumerator
sl_bt_scanner_data_status_complete

(0x0) All data of the advertisement has been reported.

sl_bt_scanner_data_status_incomplete_more

(0x1) Data of the advertisement is incomplete in this event, and more data will come in new events.

sl_bt_scanner_data_status_incomplete_nomore

(0x2) Data of the advertisement is incomplete in this event, but no more data will come, i.e., the data of the advertisement is truncated.


sl_bt_scanner_filter_policy_t#

sl_bt_scanner_filter_policy_t

The scanning filter policy setting determines which advertisements and scan responses are delivered to the application when scanning. See the Bluetooth Core specification Volume 6, Part B, Section 4.3.3 "Scanning filter policy" for a detailed description of this setting.

Note that some filter policies require the application to include additional Bluetooth feature components. Filter policies that use the Filter Accept List require that the application has included the bluetooth_feature_accept_list component. Filter policies that require the Bluetooth controller to resolve a Resolvable Private Address require that the application has included the bluetooth_feature_resolving_list component.

Enumerator
sl_bt_scanner_filter_policy_basic_unfiltered

(0x0) Advertising and scan response PDUs are processed from all devices. For directed advertising, the target address must additionally match the identity address of the local device or be a Resolvable Private Address that is resolved to the local device by the Bluetooth controller.

sl_bt_scanner_filter_policy_basic_filtered

(0x1) Advertising and scan response PDUs are processed only from devices that the application has added to the Filter Accept List. For directed advertising, the target address must additionally match the identity address of the local device or be a Resolvable Private Address that is resolved to the local device by the Bluetooth controller.

sl_bt_scanner_filter_policy_extended_unfiltered

(0x2) Advertising and scan response PDUs are processed from all devices. For directed advertising, the target address must additionally match the identity address of the local device or be any Resolvable Private Address.

sl_bt_scanner_filter_policy_extended_filtered

(0x3) Advertising and scan response PDUs are processed only from devices that the application has added to the Filter Accept List. For directed advertising, the target address must additionally match the identity address of the local device or be any Resolvable Private Address.


Function Documentation#

sl_bt_scanner_set_parameters#

sl_status_t sl_bt_scanner_set_parameters (uint8_t mode, uint16_t interval, uint16_t window)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]mode

Enum sl_bt_scanner_scan_mode_t.

Passive or active scan. Values:

  • sl_bt_scanner_scan_mode_passive (0x0): Passive scanning mode where the device only listens to advertising packets and does not transmit packets

  • sl_bt_scanner_scan_mode_active (0x1): Active scanning mode where the device sends out a scan request packet upon receiving a scannable advertising packet from a remote device and listens to the scan response packet from the remote device

  • Default : sl_bt_scanner_scan_mode_passive

uint16_t[in]interval

The time interval when the device starts its last scan until it begins the subsequent scan. In other words, how often to scan

  • Range: 0x0004 to 0xFFFF

  • Time = Value x 0.625 ms

  • Time Range: 2.5 ms to 40.96 s

  • Default : 10 ms

A variable delay occurs when switching channels at the end of each scanning interval, which is included in the scanning interval time. During the switch time, advertising packets are not received by the device. The switch time variation is use case dependent. For example, if scanning while keeping active connections, the channel switch time might be longer than when scanning without any active connections. Increasing the scanning interval reduces the amount of time in which the device can't receive advertising packets because it switches channels less often.

After every scan interval, the scanner changes the frequency at which it operates. It cycles through all three advertising channels in a round robin fashion. According to the specification, all three channels must be used by a scanner.

uint16_t[in]window

The scan window, i.e., the duration of the primary channel scan, which must be less than or equal to the interval.

  • Range: 0x0004 to 0xFFFF

  • Time = Value x 0.625 ms

  • Time Range: 2.5 ms to 40.96 s

  • Default : 10 ms

Packet reception is aborted if the scan window ends before the packet ends.

Set scan parameters for subsequent scanning operations. If the device is currently scanning, new parameters will take effect when scanning is restarted.

This command sets the scanning filter policy to the default value sl_bt_scanner_filter_policy_basic_unfiltered. Use the command sl_bt_scanner_set_parameters_and_filter to set a specific scanning filter policy.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_scanner_set_parameters_and_filter#

sl_status_t sl_bt_scanner_set_parameters_and_filter (uint8_t mode, uint16_t interval, uint16_t window, uint32_t flags, uint8_t filter_policy)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]mode

Enum sl_bt_scanner_scan_mode_t.

Passive or active scan. Values:

  • sl_bt_scanner_scan_mode_passive (0x0): Passive scanning mode where the device only listens to advertising packets and does not transmit packets

  • sl_bt_scanner_scan_mode_active (0x1): Active scanning mode where the device sends out a scan request packet upon receiving a scannable advertising packet from a remote device and listens to the scan response packet from the remote device

  • Default : sl_bt_scanner_scan_mode_passive

uint16_t[in]interval

The time interval when the device starts its last scan until it begins the subsequent scan. In other words, how often to scan

  • Range: 0x0004 to 0xFFFF

  • Time = Value x 0.625 ms

  • Time Range: 2.5 ms to 40.96 s

  • Default : 10 ms

A variable delay occurs when switching channels at the end of each scanning interval, which is included in the scanning interval time. During the switch time, advertising packets are not received by the device. The switch time variation is use case dependent. For example, if scanning while keeping active connections, the channel switch time might be longer than when scanning without any active connections. Increasing the scanning interval reduces the amount of time in which the device can't receive advertising packets because it switches channels less often.

After every scan interval, the scanner changes the frequency at which it operates. It cycles through all three advertising channels in a round robin fashion. According to the specification, all three channels must be used by a scanner.

uint16_t[in]window

The scan window, i.e., the duration of the primary channel scan, which must be less than or equal to the interval.

  • Range: 0x0004 to 0xFFFF

  • Time = Value x 0.625 ms

  • Time Range: 2.5 ms to 40.96 s

  • Default : 10 ms

Packet reception is aborted if the scan window ends before the packet ends.

uint32_t[in]flags

Additional scanner options. Value: 0 or bitmask of Option Flags to Specify Scanning Options.

uint8_t[in]filter_policy

Enum sl_bt_scanner_filter_policy_t.

The scanning filter policy to use when scanning is started. The filter policy determines which advertisements and scan responses are delivered to the application. Values:

  • sl_bt_scanner_filter_policy_basic_unfiltered (0x0): Advertising and scan response PDUs are processed from all devices. For directed advertising, the target address must additionally match the identity address of the local device or be a Resolvable Private Address that is resolved to the local device by the Bluetooth controller.

  • sl_bt_scanner_filter_policy_basic_filtered (0x1): Advertising and scan response PDUs are processed only from devices that the application has added to the Filter Accept List. For directed advertising, the target address must additionally match the identity address of the local device or be a Resolvable Private Address that is resolved to the local device by the Bluetooth controller.

  • sl_bt_scanner_filter_policy_extended_unfiltered (0x2): Advertising and scan response PDUs are processed from all devices. For directed advertising, the target address must additionally match the identity address of the local device or be any Resolvable Private Address.

  • sl_bt_scanner_filter_policy_extended_filtered (0x3): Advertising and scan response PDUs are processed only from devices that the application has added to the Filter Accept List. For directed advertising, the target address must additionally match the identity address of the local device or be any Resolvable Private Address.

  • Default : sl_bt_scanner_filter_policy_basic_unfiltered

Set scan parameters and the scanning filter policy for subsequent scanning operations. If the device is currently scanning, new parameters will take effect when scanning is restarted.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_scanner_start#

sl_status_t sl_bt_scanner_start (uint8_t scanning_phy, uint8_t discover_mode)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]scanning_phy

Enum sl_bt_scanner_scan_phy_t.

The scanning PHY(s).

In simultaneous scanning, the stack alternates the scanning on two PHYs by switching the PHY at every scan interval. When a timing parameter is set differently on 1M and Coded PHY, the stack chooses the most relaxed value for both PHYs during simultaneous scanning, i.e., the largest scan interval or the smallest scan window. If one PHY is set to passive scanning and the other to active scanning, passive scanning is chosen for simultaneous scanning. Values:

  • sl_bt_scanner_scan_phy_1m (0x1): Initiate the scanning on the 1M PHY

  • sl_bt_scanner_scan_phy_coded (0x4): Initiate the scanning on the Coded PHY

  • sl_bt_scanner_scan_phy_1m_and_coded (0x5): Simultaneous scanning by initiating the scanning on the 1M and Coded PHY alternatively

uint8_t[in]discover_mode

Enum sl_bt_scanner_discover_mode_t. Bluetooth discovery Mode. Values:

  • sl_bt_scanner_discover_limited (0x0): Discover only limited discoverable devices.

  • sl_bt_scanner_discover_generic (0x1): Discover limited and general discoverable devices.

  • sl_bt_scanner_discover_observation (0x2): Discover non-discoverable, limited and general discoverable devices.

Start the GAP discovery procedure to scan for advertising devices that use legacy or extended advertising PDUs. To cancel an ongoing discovery procedure, use the sl_bt_scanner_stop command.

If privacy is enabled, see sl_bt_gap_set_privacy_mode for the scanner private address behavior.

The invalid parameter error will be returned if the value of scanning PHYs is invalid or the device does not support a PHY.

Received advertising packets are not filtered in any way, so multiple events will be received for every advertising device in range.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events

  • sl_bt_evt_scanner_legacy_advertisement_report - This event is triggered for reporting a received advertisement that uses legacy advertising PDUs if the application includes the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component.

  • sl_bt_evt_scanner_extended_advertisement_report - This event is triggered for reporting a received advertisement that uses extended advertising PDUs if the application includes the bluetooth_feature_extended_scanner component.


sl_bt_scanner_stop#

sl_status_t sl_bt_scanner_stop (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Stop scanning for advertising devices. For more information about the discovery, see the sl_bt_scanner_start command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Macro Definition Documentation#

sl_bt_cmd_scanner_set_parameters_id#

#define sl_bt_cmd_scanner_set_parameters_id
Value:
0x06050020

sl_bt_cmd_scanner_set_parameters_and_filter_id#

#define sl_bt_cmd_scanner_set_parameters_and_filter_id
Value:
0x07050020

sl_bt_cmd_scanner_start_id#

#define sl_bt_cmd_scanner_start_id
Value:
0x03050020

sl_bt_cmd_scanner_stop_id#

#define sl_bt_cmd_scanner_stop_id
Value:
0x05050020

sl_bt_rsp_scanner_set_parameters_id#

#define sl_bt_rsp_scanner_set_parameters_id
Value:
0x06050020

sl_bt_rsp_scanner_set_parameters_and_filter_id#

#define sl_bt_rsp_scanner_set_parameters_and_filter_id
Value:
0x07050020

sl_bt_rsp_scanner_start_id#

#define sl_bt_rsp_scanner_start_id
Value:
0x03050020

sl_bt_rsp_scanner_stop_id#

#define sl_bt_rsp_scanner_stop_id
Value:
0x05050020