Persistent Store (flash)#
Persistent Store commands can be used to manage user data in PS keys in the flash memory of the Bluetooth device. User data stored within the flash memory is persistent across reset and power cycling of the device. The persistent store size is 2048 bytes. As Bluetooth bondings are also stored in this area, the space available for user data additionally depends on the number of bondings the device has at the time. The size of a Bluetooth bonding is around 150 bytes.
The maximum user data size associated to a PS key is 56 bytes.
flash commands#
flash_ps_erase#
This command can be used to erase a single PS key and its value from the persistent store.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x04 | method | Message ID |
4-5 | uint16 | key | PS key to erase |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x04 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_flash_ps_erase_rsp_t *gecko_cmd_flash_ps_erase(uint16 key);
/* Response id */
gecko_rsp_flash_ps_erase_id
/* Response structure */
struct gecko_msg_flash_ps_erase_rsp_t
{
uint16 result
}flash_ps_erase_all#
This command can be used to erase all PS keys and their corresponding values.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x00 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x01 | method | Message ID |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x01 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_flash_ps_erase_all_rsp_t *gecko_cmd_flash_ps_erase_all();
/* Response id */
gecko_rsp_flash_ps_erase_all_id
/* Response structure */
struct gecko_msg_flash_ps_erase_all_rsp_t
{
uint16 result
}flash_ps_load#
This command can be used for retrieving the value of the specified PS key.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x03 | method | Message ID |
4-5 | uint16 | key | PS key of the value to be retrieved |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x03 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x03 | method | Message ID |
4-5 | uint16 | result | Result code
|
6 | uint8array | value | The returned value of the specified PS key. |
API#
/* Function */
struct gecko_msg_flash_ps_load_rsp_t *gecko_cmd_flash_ps_load(uint16 key);
/* Response id */
gecko_rsp_flash_ps_load_id
/* Response structure */
struct gecko_msg_flash_ps_load_rsp_t
{
uint16 result,
uint8array value
}flash_ps_save#
This command can be used to store a value into the specified PS key. Allowed PS keys are in range from 0x4000 to 0x407F. At most 56 bytes user data can be stored in one PS key. Error code 0x018a (command_too_long) will be returned if more than 56 bytes data is passed in.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x03 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x02 | method | Message ID |
4-5 | uint16 | key | PS key |
6 | uint8array | value | Value to store into the specified PS key. |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x0d | class | Message class:Persistent Store |
3 | 0x02 | method | Message ID |
4-5 | uint16 | result | Result code
|
API#
/* Function */
struct gecko_msg_flash_ps_save_rsp_t *gecko_cmd_flash_ps_save(uint16 key, uint8 value_len, const uint8 *value_data);
/* Response id */
gecko_rsp_flash_ps_save_id
/* Response structure */
struct gecko_msg_flash_ps_save_rsp_t
{
uint16 result
}