Silicon Labs
bluetooth/2.13/code-examples/stack-features/security/pairing-processes-example
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
    Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/security/pairing-processes-example in 0.20 seconds
    BGAPI | BGAPI headers | Bluetooth LE | v3.3 | Silicon Labs
    https://docs.silabs.com/....
    //API Reference //BGAPI headers You are viewing documentation for version: 3.3 BGAPI# BGAPI message header format# ... BGAPI protocol stores data in little endian. ... 0x06 3 GATT Database
    GATT Server | GATT Server | Bluetooth LE | v3.2 | Silicon Labs
    https://docs.silabs.com/....
    // Bluetooth LE//Version 3.2 //API Reference ... Only (maximum BGAPI payload size - 3) amount of data can be read at once. ... See Bluetooth specification Vol 3, Part G, 7.2 for the values.
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    ... at line 1249 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.0.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    ... at line 1249 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    Connection | Bluetooth Stack API Reference | Bluetooth LE | v8.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-connect...
    ... /raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h ... /workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt ...
      Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/security/pairing-processes-example