sl_bt_evt_gatt_descriptorGATT Client#
Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
Data Structures#
struct | Data structure of the descriptor event. |
Macros#
#define | sl_bt_evt_gatt_descriptor_id 0x030900a0 Identifier of the descriptor event. |
Detailed Description#
Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
It is generated after issuing the sl_bt_gatt_discover_descriptors command.
Data Structure Documentation#
sl_bt_evt_gatt_descriptor_s#
struct sl_bt_evt_gatt_descriptor_s
Data structure of the descriptor event.
Data Fields | ||
---|---|---|
uint8_t | connection | Connection handle |
uint16_t | descriptor | GATT characteristic descriptor handle |
uuid | Descriptor UUID in little endian format |