sl_bt_evt_scanner_scan_reportScanner#
Reports an advertising or scan response packet that is received by the device's radio while in scanning mode.
Data Structures#
struct sl_bt_evt_scanner_scan_report_s
Data structure of the scan_report event.
Macros#
define sl_bt_evt_scanner_scan_report_id 0x010500a0\n#
Identifier of the scan_report event.
Detailed Description#
Reports an advertising or scan response packet that is received by the device's radio while in scanning mode.
Data Structure Documentation#
sl_bt_evt_scanner_scan_report_s#
struct sl_bt_evt_scanner_scan_report_s |
Data structure of the scan_report event.
Data Fields | ||
|---|---|---|
uint8_t | packet_type | Bits 0..2: advertising packet type
Bits 5..6: data completeness
|
address | Bluetooth address of the remote device | |
uint8_t | address_type | Advertiser address type. Values:
|
uint8_t |
| |
uint8_t | primary_phy | Enum gap_phy_type_t. The PHY on which advertising packets are transmitted on the primary advertising channel. Values:
|
uint8_t | secondary_phy | Enum gap_phy_type_t. The PHY on which advertising packets are transmitted on the secondary advertising channel. Values:
|
uint8_t | adv_sid | Advertising set identifier |
int8_t | tx_power | TX power value in the received packet header. Units: dBm
|
int8_t | rssi | Signal strength indicator (RSSI) in the last received packet. Units: dBm
|
uint8_t | channel | The channel number on which the last packet was received |
uint16_t | periodic_interval | The periodic advertising interval. Value 0 indicates no periodic advertising. Otherwise,
|
data | Advertising or scan response data | |