sl_bt_evt_system_bootSystem#
Indicates that the device has started and the radio is ready.
Data Structures#
struct | sl_bt_evt_system_boot_s Data structure of |
Macros#
#define | 0x000100a0 | |
Identifier of the boot event. |
Detailed Description#
Indicates that the device has started and the radio is ready.
This event carries the firmware build number and other software and hardware identification codes.
Data Structure Documentation#
sl_bt_evt_system_boot_s#
struct sl_bt_evt_system_boot_s
Data structure of the boot event.
Data Fields | |
|---|---|
uint16_t major | Major release version |
uint16_t minor | Minor release version |
uint16_t patch | Patch release number |
uint16_t build | Build number |
uint32_t bootloader | Bootloader version |
uint16_t hw | Hardware type |
uint32_t hash | Version hash |