sl_bt_evt_user_message_to_hostUser Messaging#
Used by the target application on a device to initiate communication and send a message to the NCP host.
Data Structures | |
|---|---|
struct | |
Data structure of the message_to_host event. | |
Macros | ||
|---|---|---|
#define | 0x00ff00a0 | |
Identifier of the message_to_host event. | ||
Detailed Description#
Used by the target application on a device to initiate communication and send a message to the NCP host.
Do not send event messages in the context of the user command handling.
Data Structure Documentation#
sl_bt_evt_user_message_to_host_s#
struct sl_bt_evt_user_message_to_host_s |
Data structure of the message_to_host event.
Data Fields | ||
|---|---|---|
message | The message | |