sl_bt_connection_role_t# sl_bt_connection_role_t Types of device roles in a Bluetooth connection. ... sl_bt_evt_connection_parameters - Triggered after new connection parameters are applied on ...
sl_bt_evt_gatt_server_attribute_value Indicates that the value of an attribute in the local GATT database was changed by a ... See Bluetooth specification Vol 3, Part G, 7.2 for the values.
// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... sl_bt_system_linklayer_config_key_set_simultaneous_scanning ... Bluetooth identity address in little endian format
sc = sl_bt_advertiser_start( advertising_set_handle, advertiser_general_discoverable, ... The sl_bt_external_signal( ) function will generate a Bluetooth stack event for the main loop to ...
Bluetooth, such as NFC. Devices that do not have a user interface can use OOB pairing to establish MITM ... 3.1.2 Device Privacy When a device is in device privacy mode, it is only concerned ...
Resource TypeApplication Notes
Results 1-5 of 5 for bluetooth/3.0/~/group-sl-bt-test