sl_bt_evt_scanner_scan_reportScanner#
Reports an advertising or scan response packet that is received by the device's radio while in scanning mode.
Data Structures | |
|---|---|
struct | |
Data structure of the scan_report event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_scanner_scan_report_id 0x010500a0 |
Identifier of the scan_report event. | |
Detailed Description#
Reports an advertising or scan response packet that is received by the device's radio while in scanning mode.
Data Structure Documentation#
sl_bt_evt_scanner_scan_report_s#
struct sl_bt_evt_scanner_scan_report_s
Data structure of the scan_report event.
Data Fields | ||
|---|---|---|
uint8_t | packet_type | Bits 0..2 : advertising packet type
Bits 3..4 : Reserved for future Bits 5..6 : data completeness
Bit 7 : legacy or extended advertising
|
address | Bluetooth address of the remote device | |
uint8_t | address_type | Advertiser address type. Values:
|
uint8_t | bonding | Bonding handle if the remote advertising device has previously bonded with the local device. Values:
|
uint8_t | primary_phy | Enum sl_bt_gap_phy_type_t. The PHY on which advertising packets are transmitted on the primary advertising channel. Ignore this field if the report is for a legacy advertising PDU. Values:
|
uint8_t | secondary_phy | Enum sl_bt_gap_phy_type_t. The PHY on which advertising packets are transmitted on the secondary advertising channel. Ignore this field if the report is for a legacy advertising PDU. Values:
|
uint8_t | adv_sid | Advertising set identifier |
int8_t | tx_power | TX power value in the received packet header. Units: dBm
|
int8_t | rssi | Signal strength indicator (RSSI) in the last received packet. Units: dBm
|
uint8_t | channel | The channel number on which the last packet was received |
uint16_t | periodic_interval | The periodic advertising interval. Value 0 indicates no periodic advertising. Otherwise,
|
data | Advertising or scan response data | |