sl_bt_evt_dfu_bootDevice Firmware Update#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Data Structures | |
|---|---|
struct | |
Data structure of the boot event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_dfu_boot_id 0x000000a0 |
Identifier of the boot event. | |
Detailed Description#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Data Structure Documentation#
sl_bt_evt_dfu_boot_s#
struct sl_bt_evt_dfu_boot_s |
Data structure of the boot event.
Data Fields | ||
|---|---|---|
uint32_t | version | The version of the bootloader |