... message types, IDs, and data payload length. Byte 1# Bits 0 - 2 : Highest 3 bits of the data payload length field Bits 3 - 5 : Device type Bit value 100 : Bluetooth LE ... 0x0d 1 Events
// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... Bluetooth identity address in little endian format ... data Data to write Write data into the system data buffer.
Bluetooth identity address in little endian format ... [in] data Data to write Write data into the system data buffer. Data will be appended to the end of existing data.
// Bluetooth LE//Version 8.1.0 //Bluetooth Stack API Reference //Connection ... Types of device roles in a Bluetooth connection. ... Used only when Bluetooth device is acting as a peripheral.
... to report detailed packet transmission and reception data, such as timestamps, link quality (or LQI), ... Capturing Data and Managing Sessions: Describes how to perform live captures, and save ...