OTA#

OTA.

Functions#


sl_status_t | sl_bt_ota_set_device_name (size_t name_len, const uint8_t *name)

sl_status_t | sl_bt_ota_set_advertising_data (uint8_t packet_type, size_t adv_data_len, const uint8_t *adv_data)

sl_status_t | sl_bt_ota_set_configuration (uint32_t flags)

sl_status_t | sl_bt_ota_set_rf_path (uint8_t enable, uint8_t antenna)

Detailed Description#

OTA.

Commands for configuring OTA DFU.

Function Documentation#

◆ sl_bt_ota_set_device_name()#

sl_status_t sl_bt_ota_set_device_name

(

size_t

name_len,

const uint8_t *

name

)

Set the device name to be used during the OTA update. The name is stored in the persistent store. Maximum name length is 17 bytes.

Default is "OTA" if a name is not set.

Parameters

[in]

name_len

Length of data in name

[in]

name

OTA device name

Returns

SL_STATUS_OK if successful. Error code otherwise.

◆ sl_bt_ota_set_advertising_data()#

sl_status_t sl_bt_ota_set_advertising_data

(

uint8_t

packet_type,

size_t

adv_data_len,

const uint8_t *

adv_data

)

Set advertising packets in OTA. Maximum 31 bytes of data can be set.

Parameters

[in]

packet_type

This value selects whether data is intended for advertising packets or scan response packets.

  • 2: OTA advertising packets

  • 4: OTA scan response packets

[in]

adv_data_len

Length of data in adv_data

[in]

adv_data

Data to be set

Returns

SL_STATUS_OK if successful. Error code otherwise.

◆ sl_bt_ota_set_configuration()#

sl_status_t sl_bt_ota_set_configuration

(

uint32_t

flags

)

Set OTA configuration. The setting is stored in the persistent store.

Parameters

 [in]| `flags`|

OTA configuration flags. This value is given as a bitmask. Flags:

Bit 0: Advertising address

  • 0: Use public device address

  • 1: Use a random address

Bit 1: Application update version check. Check the version number and product ID of the application upgrade before applying. If the version number of the current application can not be determined, this implementation will assume that it is OK to apply the new image. Note that this is not a security feature.

  • 0: Disable version check

  • 1: Enable version check

Bit 2 to 31: Reserved

Default value: 0

Returns

SL_STATUS_OK if successful. Error code otherwise.

◆ sl_bt_ota_set_rf_path()#

sl_status_t sl_bt_ota_set_rf_path

(

uint8_t

enable,

uint8_t

antenna

)

Set RF path antenna for OTA. Should be used only if device has multiple antenna ports. The setting is stored in the persistent store.

Parameters

[in]

enable

If enabled antenna selection is used in OTA, otherwise default antenna is used.

[in]

antenna

Set antenna used in OTA. Value should be come from RAIL_AntennaSel_t enum. See antenna path selection in RAIL rail_chip_specific.h.

Returns

SL_STATUS_OK if successful. Error code otherwise.