Silicon Labs
bluetooth/3.3/functions
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
    Results 1-5 of 5 for bluetooth/3.3/functions in 0.26 seconds
    GATT Server | GATT Server | Bluetooth LE | v3.2 | Silicon Labs
    https://docs.silabs.com/....
    ... client configuration was changed or whether a characteristic confirmation was received. Functions# sl_status_t | sl_bt_gatt_ ... See Bluetooth specification Vol 3, Part G, 7.2 for the values.
    BGAPI | BGAPI headers | Bluetooth LE | v3.3 | Silicon Labs
    https://docs.silabs.com/....
    // Bluetooth LE//Version 3.3 //API Reference ... 3 bits of the data payload length field Bits 3 - 5 : Device type Bit value 100 : Bluetooth LE Bit value 101 : Bluetooth Mesh Bit 6 : Reserved
    Connection | Bluetooth Stack API Reference | Bluetooth LE | v8.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-connect...
    This enum defines the flag values for a reported transmit power level. Functions# sl_status_t ... The Bluetooth stack will enter a state where it continuously scans for the connectable ...
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    sl_bt_cmd_system_start_bluetooth_id 0x1c010020 ... radiated TX power level is configured to -3 dBm and the maximum radiated TX power ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.0.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    sl_bt_cmd_system_start_bluetooth_id 0x1c010020 ... radiated TX power level is configured to -3 dBm and the maximum radiated TX power ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
      Results 1-5 of 5 for bluetooth/3.3/functions