sl_bt_evt_advertiser_timeoutAdvertiser#

Indicates the legacy or extended advertising on an advertising set has stopped because the advertiser has completed the configured number of advertising events or the advertising has reached the configured duration.

Data Structures

struct  

sl_bt_evt_advertiser_timeout_s

Data structure of the timeout event.

Macros

#define  

sl_bt_evt_advertiser_timeout_id   0x010400a0

Identifier of the timeout event.

Detailed Description#

Indicates the legacy or extended advertising on an advertising set has stopped because the advertiser has completed the configured number of advertising events or the advertising has reached the configured duration.

The maximum number of advertising events or advertising duration can be configured by the maxevents or duration parameter in the command sl_bt_advertiser_set_timing.


Data Structure Documentation#

◆sl_bt_evt_advertiser_timeout_s#

struct sl_bt_evt_advertiser_timeout_s

Data structure of the timeout event.

Data Fields

uint8_t

handle

The advertising set handle