sl_bt_evt_gatt_server_execute_write_completedGATT Server#

Indicates that the execute write command from a remote GATT client has completed with the given result.

Data Structures

struct  

sl_bt_evt_gatt_server_execute_write_completed_s

Data structure of the execute_write_completed event.

Macros

#define  

sl_bt_evt_gatt_server_execute_write_completed_id   0x040a00a0

Identifier of the execute_write_completed event.

Detailed Description#

Indicates that the execute write command from a remote GATT client has completed with the given result.


Data Structure Documentation#

◆sl_bt_evt_gatt_server_execute_write_completed_s#

struct sl_bt_evt_gatt_server_execute_write_completed_s

Data structure of the execute_write_completed event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint16_t

result

Execute write result