Periodic Advertising Configuration FlagsPeriodic Advertiser#

Macros

#define 

SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER   0x1

#define 

SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING   0x2

Detailed Description#

Defines configuration flags for periodic advertising.

Macro Definition Documentation#

◆SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER#

#define SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER   0x1

Include the TX power in advertising packets.

◆SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING#

#define SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING   0x2

Automatically start the extended advertising on the advertising set. The advertising will be started in non-connectable and non-scannable mode.