sl_bt_evt_scanner_legacy_advertisement_reportScanner#

Reports an advertising data or scan response packet from an advertising device that uses legacy advertising PDUs.

Data Structures

struct  

sl_bt_evt_scanner_legacy_advertisement_report_s

Data structure of the legacy_advertisement_report event.

Macros

#define  

sl_bt_evt_scanner_legacy_advertisement_report_id   0x000500a0

Identifier of the legacy_advertisement_report event.

Detailed Description#

Reports an advertising data or scan response packet from an advertising device that uses legacy advertising PDUs.

This event is used to report advertisements only if the application includes the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component

Otherwise, the sl_bt_evt_scanner_scan_report event is used for maintaining the backwards compatibility.


Data Structure Documentation#

◆sl_bt_evt_scanner_legacy_advertisement_report_s#

struct sl_bt_evt_scanner_legacy_advertisement_report_s

Data structure of the legacy_advertisement_report event.

Data Fields

name

description

uint8_t

event_flags

The event type flag(s) in the advertisement packet. Value: One or more flags defined in Event Type Flags of Advertisement Reports

bd_addr

address

Advertiser address

uint8_t

address_type

Advertiser address type. Values:

  • 0: Public address

  • 1: Random address

uint8_t

bonding

Bonding handle if the remote advertising device has previously bonded with the local device. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle

int8_t

rssi

Signal strength indicator (RSSI) in the last received packet. Units: dBm

  • Range: -127 to +20

uint8_t

channel

The channel number on which the last packet was received

bd_addr

target_address

The target address if the advertisement is from directed advertising, otherwise ignored

uint8_t

target_address_type

The target address type if the advertisement is from directed advertising, otherwise ignored. Values:

  • 0: Public address

  • 1: Random address

uint8array

data

Advertising or scan response data. Ignore if this is directed advertising.