sl_bt_evt_test_dtm_completedTesting Commands#

Indicates that the radio has processed a test start or end command.

Data Structures

struct  

sl_bt_evt_test_dtm_completed_s

Data structure of the dtm_completed event.

Macros

#define  

sl_bt_evt_test_dtm_completed_id   0x000e00a0

Identifier of the dtm_completed event.

Detailed Description#

Indicates that the radio has processed a test start or end command.

The result parameter indicates the success of the command.

After the receiver or transmitter test is stopped, the number_of_packets parameter in this event indicates the number of received or transmitted packets.


Data Structure Documentation#

◆sl_bt_evt_test_dtm_completed_s#

struct sl_bt_evt_test_dtm_completed_s

Data structure of the dtm_completed event.

Data Fields

name

description

uint16_t

result

Command result

uint16_t

number_of_packets

Number of packets Only valid for sl_bt_test_dtm_end command.