sl_bt_evt_user_message_to_hostUser Messaging#

Used by the target application on a device to initiate communication and send a message to the NCP host.

Data Structures

struct  

sl_bt_evt_user_message_to_host_s

Data structure of the message_to_host event.

Macros

#define  

sl_bt_evt_user_message_to_host_id   0x00ff00a0

Identifier of the message_to_host event.

Detailed Description#

Used by the target application on a device to initiate communication and send a message to the NCP host.

Do not send event messages in the context of the user command handling.


Data Structure Documentation#

◆sl_bt_evt_user_message_to_host_s#

struct sl_bt_evt_user_message_to_host_s

Data structure of the message_to_host event.

Data Fields

name

description

uint8array

message

The message