sl_bt_evt_dfu_boot_failureDevice Firmware Update#

This event indicates that an error, which prevents the device from booting, has occurred in bootloader.

Data Structures

struct  

sl_bt_evt_dfu_boot_failure_s

Data structure of the boot_failure event.

Macros

#define 

sl_bt_evt_dfu_boot_failure_id   0x010000a0

Identifier of the boot_failure event.

Detailed Description#

This event indicates that an error, which prevents the device from booting, has occurred in bootloader.


Data Structure Documentation#

◆sl_bt_evt_dfu_boot_failure_s#

struct sl_bt_evt_dfu_boot_failure_s

Data structure of the boot_failure event.

Data Fields

uint16_t

reason

The reason for boot failure.