Modules#

throughput_central_characteristic_t

throughput_central_characteristic_found_t

Throughput Test Receiver (Central) Role API#

Throughput Test Receiver (Central) Role API opens connection to Throughput Test Transmitter (Peripheral) Role nodes, registers to notifications or indications. Throughput parameters can be managed using the API calls or via CLI. The API provides interface for configuring, starting and stopping transmission. Status and result callbacks can be also registered using the API.

Functions#

bool
sl_status_t
throughput_central_set_mode(throughput_mode_t mode, uint32_t amount)
sl_status_t
sl_status_t
throughput_central_set_tx_power(throughput_tx_power_t tx_power, bool power_control, bool deep_sleep)
sl_status_t
throughput_central_set_connection_parameters(throughput_time_t min_interval, throughput_time_t max_interval, throughput_time_t latency, throughput_time_t timeout)
sl_status_t
throughput_central_set_type(throughput_notification_t type)
sl_status_t
sl_status_t
sl_status_t
throughput_central_set_scan_phy(throughput_scan_phy_t phy)
sl_status_t
void
bt_on_event_central(sl_bt_msg_t *evt)
void
throughput_central_on_role_set(throughput_role_t role)
void
throughput_central_on_state_change(throughput_state_t state)
void
throughput_central_on_mode_change(throughput_mode_t mode)
void
throughput_central_on_finish(throughput_value_t throughput, throughput_count_t count, throughput_count_t lost, throughput_count_t error, throughput_time_t time)
void
throughput_central_on_transmit_power_change(throughput_tx_power_t power)
void
throughput_central_on_rssi_change(throughput_rssi_t rssi)
void
throughput_central_on_phy_change(throughput_phy_t phy)
void
throughput_central_on_notification_change(throughput_notification_t notification)
void
throughput_central_on_indication_change(throughput_notification_t indication)
void
throughput_central_on_result_indication_change(throughput_notification_t result)
void
throughput_central_on_data_size_change(throughput_pdu_size_t data_size)
void
throughput_central_on_connection_settings_change(throughput_pdu_size_t pdu, throughput_mtu_size_t mtu)
void
throughput_central_on_connection_timings_change(throughput_time_t interval, throughput_time_t latency, throughput_time_t timeout)
void
throughput_central_on_characteristics_found(throughput_central_characteristic_found_t characteristics)
void
throughput_central_on_discovery_state_change(throughput_discovery_state_t state)
float
throughput_central_calculate(throughput_value_t *throughput)
bool
throughput_central_decode_address(char *addess_str, uint8_t *address)
float

Function Documentation#

throughput_central_allowlist_add#

bool throughput_central_allowlist_add (uint8_t * address)
Parameters
TypeDirectionArgument NameDescription
uint8_t *[in]address

BT address in 6 byte format

Add an address to the allowlist. Returns

  • true if adding the address was successful


throughput_central_allowlist_clear#

bool throughput_central_allowlist_clear (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Clear the allowlist Returns

  • true if adding the clear was succesful


throughput_central_enable#

void throughput_central_enable (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Enable receiver.


throughput_central_disable#

sl_status_t throughput_central_disable (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Disable receiver.


throughput_central_set_mode#

sl_status_t throughput_central_set_mode (throughput_mode_t mode, uint32_t amount)
Parameters
TypeDirectionArgument NameDescription
throughput_mode_t[in]mode

the transmission mode is either of:

  • THROUGHPUT_MODE_CONTINUOUS: transfer until stop

  • THROUGHPUT_MODE_FIXED_TIME: transfer data for a fixed time

  • THROUGHPUT_MODE_FIXED_LENGTH: a fixed amount of data to transfer

uint32_t[in]amount

the time in ms or data in bytes to transfer

Set receiver mode. Returns

  • status of the operation


throughput_central_set_mtu_size#

sl_status_t throughput_central_set_mtu_size (uint8_t mtu)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]mtu

MTU size in bytes

Set data sizes for reception. Returns

  • status of the operation


throughput_central_set_tx_power#

sl_status_t throughput_central_set_tx_power (throughput_tx_power_t tx_power, bool power_control, bool deep_sleep)
Parameters
TypeDirectionArgument NameDescription
throughput_tx_power_t[in]tx_power

requested tx power in dBm

bool[in]power_control

enable adaptive power control

bool[in]deep_sleep

enable deep sleep during test

Set transmission power. Returns

  • status of the operation


throughput_central_set_connection_parameters#

sl_status_t throughput_central_set_connection_parameters (throughput_time_t min_interval, throughput_time_t max_interval, throughput_time_t latency, throughput_time_t timeout)
Parameters
TypeDirectionArgument NameDescription
throughput_time_t[in]min_interval

Minimum connection interval (in 1.25 ms steps)

throughput_time_t[in]max_interval

Maximum connection interval (in 1.25 ms steps)

throughput_time_t[in]latency

Responder latency (in connection intervals)

throughput_time_t[in]timeout

Supervision timeout (in 10 ms steps)

Set connection parameters. Returns

  • status of the operation


throughput_central_set_type#

sl_status_t throughput_central_set_type (throughput_notification_t type)
Parameters
TypeDirectionArgument NameDescription
throughput_notification_t[in]type

type of the test (notification or indication)

Set type of transmission. Returns

  • status of the operation


throughput_central_start#

sl_status_t throughput_central_start (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Start transmission on remote side. Returns

  • status of the operation


throughput_central_stop#

sl_status_t throughput_central_stop (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Stop transmission on remote side. Returns

  • status of the operation


throughput_central_set_scan_phy#

sl_status_t throughput_central_set_scan_phy (throughput_scan_phy_t phy)
Parameters
TypeDirectionArgument NameDescription
throughput_scan_phy_t[in]phy

PHY used for scanning

Set PHY used for scanning. Returns

  • status of the operation


throughput_central_set_connection_phy#

sl_status_t throughput_central_set_connection_phy (throughput_phy_t phy)
Parameters
TypeDirectionArgument NameDescription
throughput_phy_t[in]phy

PHY used for the connection

Set PHY used for connection. Returns

  • status of the operation


throughput_central_change_phy#

sl_status_t throughput_central_change_phy (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Change PHY to next one.

  • In case of scanning, it is used for changing between CODED and 1M PHY

  • In a connection, it is used to change between 1M, 2M and CODED PHYs Returns

    • status of the operation


throughput_central_step#

void throughput_central_step (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Process step for throughput central.


bt_on_event_central#

void bt_on_event_central (sl_bt_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_bt_msg_t *[in]evt

Event coming from the Bluetooth stack.

Bluetooth stack event handler.


throughput_central_on_role_set#

void throughput_central_on_role_set (throughput_role_t role)
Parameters
TypeDirectionArgument NameDescription
throughput_role_t[in]role

the role can be only THROUGHPUT_ROLE_PERIPHERAL

Callback to handle role settings. Note

  • To be implemented in user code.


throughput_central_on_state_change#

void throughput_central_on_state_change (throughput_state_t state)
Parameters
TypeDirectionArgument NameDescription
throughput_state_t[in]state

current state

Callback to handle state change. Note

  • To be implemented in user code.


throughput_central_on_mode_change#

void throughput_central_on_mode_change (throughput_mode_t mode)
Parameters
TypeDirectionArgument NameDescription
throughput_mode_t[in]mode

current mode

Callback to handle mode change. Note

  • To be implemented in user code.


throughput_central_on_start#

void throughput_central_on_start (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Callback to handle transmission start event. Note

  • To be implemented in user code.


throughput_central_on_finish#

void throughput_central_on_finish (throughput_value_t throughput, throughput_count_t count, throughput_count_t lost, throughput_count_t error, throughput_time_t time)
Parameters
TypeDirectionArgument NameDescription
throughput_value_t[in]throughput

throughput value in bits/second (bps)

throughput_count_t[in]count

data volume transmitted, in bytes

throughput_count_t[in]lost

number of packets lost

throughput_count_t[in]error

number of wrong packets

throughput_time_t[in]time

total measurement time

Callback to handle transmission finished event. Note

  • To be implemented in user code.


throughput_central_on_transmit_power_change#

void throughput_central_on_transmit_power_change (throughput_tx_power_t power)
Parameters
TypeDirectionArgument NameDescription
throughput_tx_power_t[in]power

tx power in dBm

Callback to handle tx power changed event. Note

  • To be implemented in user code.


throughput_central_on_rssi_change#

void throughput_central_on_rssi_change (throughput_rssi_t rssi)
Parameters
TypeDirectionArgument NameDescription
throughput_rssi_t[in]rssi

RSSI value

Callback to handle RSSI changed event. Note

  • To be implemented in user code.


throughput_central_on_phy_change#

void throughput_central_on_phy_change (throughput_phy_t phy)
Parameters
TypeDirectionArgument NameDescription
throughput_phy_t[in]phy

PHY that is in use

Callback to handle phy changed event. Note

  • To be implemented in user code.


throughput_central_on_notification_change#

void throughput_central_on_notification_change (throughput_notification_t notification)
Parameters
TypeDirectionArgument NameDescription
throughput_notification_t[in]notification

notification status

Callback to handle notification changed event. Note

  • To be implemented in user code.


throughput_central_on_indication_change#

void throughput_central_on_indication_change (throughput_notification_t indication)
Parameters
TypeDirectionArgument NameDescription
throughput_notification_t[in]indication

indication status

Callback to handle indication changed event. Note

  • To be implemented in user code.


throughput_central_on_result_indication_change#

void throughput_central_on_result_indication_change (throughput_notification_t result)
Parameters
TypeDirectionArgument NameDescription
throughput_notification_t[in]result

result indication status

Callback to handle result indication changed event. Note

  • To be implemented in user code.


throughput_central_on_data_size_change#

void throughput_central_on_data_size_change (throughput_pdu_size_t data_size)
Parameters
TypeDirectionArgument NameDescription
throughput_pdu_size_t[in]data_size

Data size in bytes

Callback to handle data size change when receiving data. Note

  • To be implemented in user code.


throughput_central_on_connection_settings_change#

void throughput_central_on_connection_settings_change (throughput_pdu_size_t pdu, throughput_mtu_size_t mtu)
Parameters
TypeDirectionArgument NameDescription
throughput_pdu_size_t[in]pdu

PDU size in bytes

throughput_mtu_size_t[in]mtu

MTU size in bytes

Callback to handle connection parameter changes. Note

  • To be implemented in user code.


throughput_central_on_connection_timings_change#

void throughput_central_on_connection_timings_change (throughput_time_t interval, throughput_time_t latency, throughput_time_t timeout)
Parameters
TypeDirectionArgument NameDescription
throughput_time_t[in]interval

Connection interval (in 1.25 ms steps)

throughput_time_t[in]latency

Responder latency (in connection intervals)

throughput_time_t[in]timeout

Supervision timeout (in 10 ms steps)

Callback to handle connection timing changes. Note

  • To be implemented in user code.


throughput_central_on_characteristics_found#

void throughput_central_on_characteristics_found (throughput_central_characteristic_found_t characteristics)
Parameters
TypeDirectionArgument NameDescription
throughput_central_characteristic_found_t[in]characteristics

Found characteristics

Callback to handle characteristic found event. Note

  • To be implemented in user code.


throughput_central_on_discovery_state_change#

void throughput_central_on_discovery_state_change (throughput_discovery_state_t state)
Parameters
TypeDirectionArgument NameDescription
throughput_discovery_state_t[in]state

State of the discovery

Callback to handle discovery state change. Note

  • To be implemented in user code.


throughput_central_calculate#

float throughput_central_calculate (throughput_value_t * throughput)
Parameters
TypeDirectionArgument NameDescription
throughput_value_t *[out]throughput

calculated throughput value

Calculate throughput. Returns

  • the elapsed time in seconds since measurement started


throughput_central_decode_address#

bool throughput_central_decode_address (char * addess_str, uint8_t * address)
Parameters
TypeDirectionArgument NameDescription
char *[in]addess_str

Address string

uint8_t *[out]address

address byte array

Convert address string to address data bytes. Returns

  • true if operation was successful


waiting_indication#

void waiting_indication (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ASCII graphics for indicating wait status


timer_start#

void timer_start ()

Start timer


timer_end#

float timer_end ()

Timer end. The return value of this function shall be the time passed form the timer_start() call in seconds.


timer_refresh_rssi_start#

void timer_refresh_rssi_start (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Start RSSI refresh timer


timer_refresh_rssi_stop#

void timer_refresh_rssi_stop (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Stop RSSI refresh timer


timer_on_refresh_rssi#

void timer_on_refresh_rssi (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Event handler


Macro Definition Documentation#

THROUGHPUT_CENTRAL_TEST_TYPE#

#define THROUGHPUT_CENTRAL_TEST_TYPE
Value:
sl_bt_gatt_notification

THROUGHPUT_CENTRAL_MODE_DEFAULT#

#define THROUGHPUT_CENTRAL_MODE_DEFAULT
Value:
THROUGHPUT_MODE_CONTINUOUS

THROUGHPUT_CENTRAL_FIXED_DATA_SIZE#

#define THROUGHPUT_CENTRAL_FIXED_DATA_SIZE
Value:
100000

THROUGHPUT_CENTRAL_FIXED_TIME#

#define THROUGHPUT_CENTRAL_FIXED_TIME
Value:
10000

THROUGHPUT_CENTRAL_MTU_SIZE#

#define THROUGHPUT_CENTRAL_MTU_SIZE
Value:
247

THROUGHPUT_DEFAULT_SCAN_PHY#

#define THROUGHPUT_DEFAULT_SCAN_PHY
Value:
sl_bt_scanner_scan_phy_1m

THROUGHPUT_DEFAULT_PHY#

#define THROUGHPUT_DEFAULT_PHY
Value:
sl_bt_gap_phy_coding_1m_uncoded

THROUGHPUT_CENTRAL_CONNECTION_INTERVAL_MIN#

#define THROUGHPUT_CENTRAL_CONNECTION_INTERVAL_MIN
Value:
32

THROUGHPUT_CENTRAL_CONNECTION_INTERVAL_MAX#

#define THROUGHPUT_CENTRAL_CONNECTION_INTERVAL_MAX
Value:
32

THROUGHPUT_CENTRAL_CONNECTION_RESPONDER_LATENCY#

#define THROUGHPUT_CENTRAL_CONNECTION_RESPONDER_LATENCY
Value:
0

THROUGHPUT_CENTRAL_CONNECTION_TIMEOUT#

#define THROUGHPUT_CENTRAL_CONNECTION_TIMEOUT
Value:
1000

THROUGHPUT_CENTRAL_TX_POWER#

#define THROUGHPUT_CENTRAL_TX_POWER
Value:
10

THROUGHPUT_CENTRAL_POWER_CONTROL_ENABLE#

#define THROUGHPUT_CENTRAL_POWER_CONTROL_ENABLE
Value:
0

THROUGHPUT_CENTRAL_SLEEP_ENABLE#

#define THROUGHPUT_CENTRAL_SLEEP_ENABLE
Value:
0

THROUGHPUT_CENTRAL_ALLOWLIST_ENABLE#

#define THROUGHPUT_CENTRAL_ALLOWLIST_ENABLE
Value:
0

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_1_ENABLE#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_1_ENABLE
Value:
0

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_1#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_1
Value:
"00:00:00:00:00:00"

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_2_ENABLE#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_2_ENABLE
Value:
0

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_2#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_2
Value:
"00:00:00:00:00:00"

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_3_ENABLE#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_3_ENABLE
Value:
0

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_3#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_3
Value:
"00:00:00:00:00:00"

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_4_ENABLE#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_4_ENABLE
Value:
0

THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_4#

#define THROUGHPUT_CENTRAL_ALLOWLIST_SLOT_4
Value:
"00:00:00:00:00:00"

THROUGHPUT_CENTRAL_CHARACTERISTICS_ALL#

#define THROUGHPUT_CENTRAL_CHARACTERISTICS_ALL
Value:
0x0F

ADR_LEN#

#define ADR_LEN
Value:
6

THROUGHPUT_CENTRAL_REFRESH_TIMER_PERIOD#

#define THROUGHPUT_CENTRAL_REFRESH_TIMER_PERIOD
Value:
1000