ESL Tag core#

Implements the ESL Tag role of the Bluetooth Electronic Shelf Label Profile. It contains the mandatory ESL Tag characteristics, only. Optional features has to be added to the project as separate components, if needed. This component implements all the core functionalities, while also declares the interface of the optional features (and provides the WEAK implementations for them). This is a No-Code component, any additional feature can be added as a component.

Typedefs#

typedef uint8_t

ESL Display Info Display Type.

typedef struct esl_display_info_t *

ESL Display Info first class abstract data pointer type.

typedef uint8_t
typedef uint8_t

ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.

typedef uint8_t

ESL LED type.

typedef uint8_t

ESL LED color gamut control type.

typedef uint16_t

ESL LED repeats type.

typedef uint8_t
typedef uint8_t
typedef uint8_t

Functions#

sl_status_t
sl_status_t
void *
esl_core_encrypt_message(void *msg, uint8_t *len)
void *
esl_core_decrypt_message(void *msg, uint8_t *len)
sl_status_t
esl_display_refresh(uint8_t display_index, uint8_t *image_index)
sl_status_t
esl_display_update(uint8_t display_index, uint8_t image_index)
esl_error_t
void
esl_core_set_last_error(esl_error_t error_code)
void
sl_status_t
esl_image_get_data(uint8_t image_index, uint16_t *offset, uint16_t buf_size, uint8_t *target_buf)
uint8_t
typedef(struct { uint8_t data[5];uint8_t bit_off_period;uint8_t bit_on_period;}) esl_led_flashing_pattern_t

ESL LED flashing pattern ESL Service Spec. d09r18, Section 3.10.2.10.2.2.

typedef(struct { uint8_t index;esl_led_gamut_control_t gamut;esl_led_flashing_pattern_t pattern;esl_led_repeats_type_t repeats;}) esl_led_control_t

ESL LED Control parameter, ESL Service Spec. d09r18, Section 3.10.2.10.1.

void
sl_status_t
esl_led_control(esl_led_control_t *control_param)
bool
esl_led_is_srgb(uint8_t led_index)
sl_status_t
esl_core_build_response(tlv_t tlv, const void *input_data)
uint8_t
esl_core_get_responses(uint8_t remaining_length, uint8_t *buf_p)
void
sl_status_t
esl_sensor_read(uint8_t index)
sl_status_t
esl_display_create(uint16_t width, uint16_t height, esl_display_type_t type, esl_display_info_p *info)
sl_status_t
esl_display_add(esl_display_info_p info, esl_va_method_p init_func, esl_va_method_p write_func)
void
esl_display_bt_on_event(sl_bt_msg_t *evt)
sl_status_t
esl_display_set_image(uint8_t display_index, uint8_t image_index)
sl_status_t
esl_display_get_width(uint8_t display_index, uint16_t *width)
sl_status_t
esl_display_get_height(uint8_t display_index, uint16_t *height)
sl_status_t
esl_display_get_type(uint8_t display_index, esl_display_type_t *type)
sl_status_t
esl_led_add(esl_led_type_t type, uint8_t red_value, uint8_t green_value, uint8_t blue_value)
sl_status_t
esl_led_on(uint8_t led_index, esl_led_gamut_control_t gamut)
sl_status_t
esl_led_off(uint8_t led_index)
esl_led_create_color(uint8_t red_value, uint8_t green_value, uint8_t blue_value, uint8_t brightness)
void
esl_led_bt_on_event(sl_bt_msg_t *evt)

Macros#

#define
ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MS (ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MIN * 60 * 1000)
#define

Definition for unknown battery voltage level (an implausible value)

#define

ESL Display Type Assigned Numbers.

#define
ESL_ERROR_UNSPECIFIED ((esl_error_t)0x01)

Unspecified Error: any error condition that is not covered by a specific error code below

#define
ESL_ERROR_INVALID_OPCODE ((esl_error_t)0x02)

Invalid Opcode: The opcode was not recognized.

#define
ESL_ERROR_INVALID_STATE ((esl_error_t)0x03)

Invalid State: The request was not valid for the present ESL state.

#define
ESL_ERROR_INVALID_IMAGE_INDEX ((esl_error_t)0x04)

Invalid Image Index: The Image_Index value was out of range.

#define
ESL_ERROR_IMAGE_NOT_AVAILABLE ((esl_error_t)0x05)

Image Not Available: The requested image contained no image data.

#define
ESL_ERROR_INVALID_PARAMETER ((esl_error_t)0x06)

Invalid Parameter(s): The parameter value(s) or length did not match the opcode

#define
ESL_ERROR_CAPACITY_LIMIT ((esl_error_t)0x07)

Capacity Limit: The required response could not be sent as it would exceed the payload size limit

#define
ESL_ERROR_INSUFFICIENT_BATTERY ((esl_error_t)0x08)

Insufficient Battery: The request could not be processed because of a lack of battery charge

#define

Insufficient Resources: The request could not be processed because of a lack of resources. This may be a temporary condition.

#define
ESL_ERROR_RETRY ((esl_error_t)0x0A)

Retry: The ESL is temporarily not able to give a full response (e.g., because the required sensor hardware was asleep) and the AP is asked to try the same command again.

#define
ESL_ERROR_QUEUE_FULL ((esl_error_t)0x0B)

Queue Full: The ESL is temporarily unable to add a further timed command to the queue of pending commands ­the queue has reached its limit.

#define
ESL_ERROR_IMPLAUSIBLE_TIME ((esl_error_t)0x0C)

Implausible time: The Absolute Time parameter value in the command would result in a delay longer than 48 days (that is, it's a possible overflow)

#define
ESL_ERROR_VENDOR_NOERROR ((esl_error_t)0xFF)

No Error: 0xFF is reserved for 'no error' indication. For internal use only, and it is Silicon Labs specific.

#define
ESL_ERROR_VENDOR_NOREPORT ((esl_error_t)0xFE)

No report: 0xFE is reserved for 'no error report needed for timed commands' indication. For internal use only, and it is Silicon Labs specific.

#define

Wrapper around esl_core_set_last_error() to clear the last error

#define

Wrapper around esl_core_get_last_error() to check if there's no error

#define

ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.

#define
ESL_LED_TYPE_SHIFT ((esl_led_type_t)6)
#define
ESL_LED_BRIGHTNESS_SHIFT ((esl_led_gamut_control_t)6)
#define
ESL_LED_RED_GAMUT_SHIFT ((esl_led_gamut_control_t)0)
#define
ESL_LED_GREEN_GAMUT_SHIFT ((esl_led_gamut_control_t)2)
#define
ESL_LED_BLUE_GAMUT_SHIFT ((esl_led_gamut_control_t)4)
#define
ESL_LED_REPEATS_TYPE_MASK ((esl_led_repeats_type_t)0x0001)
#define
ESL_LED_REPEATS_TYPE_COUNT ((esl_led_repeats_type_t)0x0000)
#define
ESL_LED_REPEATS_TYPE_TIME ((esl_led_repeats_type_t)0x0001)
#define
ESL_LED_REPEATS_DURATION_SHIFT ((esl_led_repeats_type_t)0x0001)
#define
ESL_LED_TYPE_SRGB ((esl_led_type_t)(0x00 << ESL_LED_TYPE_SHIFT))

ESL LED type definition: sRGB.

#define
ESL_LED_TYPE_MONOCHROME ((esl_led_type_t)(0x01 << ESL_LED_TYPE_SHIFT))

ESL LED type definition: Monochrome.

#define
ESL_LED_TYPE_MASK ((esl_led_type_t)0xC0)
#define
ESL_LED_GENERIC_2BIT_MASK ((esl_led_type_t)0x03)
#define

ESL LED color gamut / brightness values.

#define
#define
#define
#define

ESL LED color gamut / brightness step percentage.

#define

Function like macro getter for 2-bit brightness value from a gamut value Returns

  • esl_led_gamut_control_t brightness

#define

Function like macro getter for 2-bit red value from a gamut value Returns

  • esl_led_gamut_control_t red value

#define

Function like macro getter for 2-bit green value from a gamut value Returns

  • esl_led_gamut_control_t green value

#define

Function like macro getter for 2-bit blue value from a gamut value Returns

  • esl_led_gamut_control_t blue value

#define

The command could not be processed successfully.

#define

Acknowledgment of a request to control an LED.

#define

General acknowledgment containing ESL status data.

#define

Acknowledgment of a request to display an image.

#define

Sensor report.

#define

Response data as specified by the vendor of the ESL.

#define
ESL_TLV_TAG_MASK ((tlv_t)0x0F)

Mask for getting the Tag value from an ESL TLV.

#define
ESL_TLV_LEN_MASK ((tlv_t)0xF0)

Mask for getting the Length value from an ESL TLV.

#define

Function like macro getter for 'Tag' field from an ESL TLV Returns

  • tlv_tag_t 'Tag' value of the TLV

#define

Function like macro getter for real 'Length' value from an ESL TLV Returns

  • tlv_length_t 'Length' value of the TLV

#define

Function like macro for setting the 'Tag' value of a TLV

#define

Function like macro for setting the 'Length' value of a TLV

#define

ESL Display extra parameters count for init_func esl_va_method function.

#define

ESL Display extra parameters count for write_func esl_va_method function.

Typedef Documentation#

esl_display_type_t#

typedef uint8_t esl_display_type_t

ESL Display Info Display Type.


esl_display_info_p#

typedef struct esl_display_info_t* esl_display_info_p

ESL Display Info first class abstract data pointer type.


esl_error_t#

typedef uint8_t esl_error_t

esl_image_object_id_t#

typedef uint8_t esl_image_object_id_t[6] [6]

ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.


esl_led_type_t#

typedef uint8_t esl_led_type_t

ESL LED type.


esl_led_gamut_control_t#

typedef uint8_t esl_led_gamut_control_t

ESL LED color gamut control type.


esl_led_repeats_type_t#

typedef uint16_t esl_led_repeats_type_t

ESL LED repeats type.


tlv_t#

typedef uint8_t tlv_t

tlv_tag_t#

typedef uint8_t tlv_tag_t

tlv_length_t#

typedef uint8_t tlv_length_t

Function Documentation#

esl_sensor_battery_init#

sl_status_t esl_sensor_battery_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

esl_sensor_battery_read#

sl_status_t esl_sensor_battery_read (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

esl_sensor_get_battery_voltage_mv#

uint32_t esl_sensor_get_battery_voltage_mv (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

esl_sensor_core_check_battery_level#

void esl_sensor_core_check_battery_level (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

esl_core_encrypt_message#

void * esl_core_encrypt_message (void * msg, uint8_t * len)
Parameters
TypeDirectionArgument NameDescription
void *[in]msg

Pointer to the message to be encrypted

uint8_t *N/Alen

len Pointer to a variable containing the length of the message to be encrypted [in bytes]

Message encryption function Returns

  • void* Pointer to the encrypted message on success, NULL otherwise.

Note

  • Also changes the value of *len to the resulting length on successful operation.


esl_core_decrypt_message#

void * esl_core_decrypt_message (void * msg, uint8_t * len)
Parameters
TypeDirectionArgument NameDescription
void *[in]msg

Pointer to the message to be decrypted

uint8_t *N/Alen

len Pointer to a variable containing the length of the message to be decrypted [in bytes]

Message decryption function Returns

  • void* Pointer to the decrypted message on success, NULL otherwise.

Note

  • Also changes the value of *len to the resulting length on successful operation.


esl_display_init#

void esl_display_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ESL Tag display component init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.


esl_display_refresh#

sl_status_t esl_display_refresh (uint8_t display_index, uint8_t * image_index)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]display_index

Selects the display to show the image on.

uint8_t *[out]image_index

Returns last image set on the refreshed display.

Refresh the content of the ESL Tag Display. Re-displays the image which was previously set on the given screen. Returns

  • sl_status_t


esl_display_update#

sl_status_t esl_display_update (uint8_t display_index, uint8_t image_index)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]display_index

Selects the display to show the image on.

uint8_t[in]image_index

Selects the image to be shown on the display.

Update image data on ESL Tag Display. Returns

  • sl_status_t


esl_display_get_count#

uint8_t esl_display_get_count ()

ESL Display: display count getter Returns

  • Number of available displays


esl_core_get_last_error#

esl_error_t esl_core_get_last_error (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Gets the last error code Returns

  • esl_error_t_t


esl_core_set_last_error#

void esl_core_set_last_error (esl_error_t error_code)
Parameters
TypeDirectionArgument NameDescription
esl_error_t[in]error_code

error code

Sets the last error code


esl_image_init#

void esl_image_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ESL Tag image init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.


esl_image_characteristic_update#

void esl_image_characteristic_update (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ESL Tag image characteristic update. ESL Core component will call this automatically on the bluetooth stack boot event. The real implementation in the ESL Tag Image component will get the display info and write it to the ESL Image Information Characteristic value for the lifecycle of the tag.


esl_image_get_data#

sl_status_t esl_image_get_data (uint8_t image_index, uint16_t * offset, uint16_t buf_size, uint8_t * target_buf)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]image_index

image_index Index of the image to get raw data chunk of

uint16_t *[out]offset

*offset Size of data already read out

uint16_t[in]buf_size

buf_size Actual size of the target buffer

uint8_t *[out]target_buf

*target_buf Buffer address to copy the image chunk into

Getter for an ESL Tag image raw data chunk

Note

  • To get full image data this function needs to be called repeatedly until the offset value increases - offset in caller has to be persistent during the process, and usually its value must be set to 0, initially

Returns

  • sl_status_t


esl_image_get_count#

uint8_t esl_image_get_count (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ESL Tag maximum image count getter Returns

  • Number of available images

Note

  • : To be implemented with each custom image storage implementation!


esl_image_reset_storage#

void esl_image_reset_storage (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Reset image storage objects Note

  • : To be implemented with each custom image storage implementation!


typedef#

typedef (struct { uint8_t data[5];uint8_t bit_off_period;uint8_t bit_on_period;} )

ESL LED flashing pattern ESL Service Spec. d09r18, Section 3.10.2.10.2.2.

Parameters
TypeDirectionArgument NameDescription
struct { uint8_t data[5];uint8_t bit_off_period;uint8_t bit_on_period;}N/A

typedef#

typedef (struct { uint8_t index;esl_led_gamut_control_t gamut;esl_led_flashing_pattern_t pattern;esl_led_repeats_type_t repeats;} )

ESL LED Control parameter, ESL Service Spec. d09r18, Section 3.10.2.10.1.

Parameters
TypeDirectionArgument NameDescription
struct { uint8_t index;esl_led_gamut_control_t gamut;esl_led_flashing_pattern_t pattern;esl_led_repeats_type_t repeats;}N/A

esl_led_init#

void esl_led_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ESL Tag LED init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.


esl_led_control#

sl_status_t esl_led_control (esl_led_control_t * control_param)
Parameters
TypeDirectionArgument NameDescription
esl_led_control_t *[in]control_param

ESL LED control parameters defined by the ESL standard - excluding the ESL ID.

ESL Tag LED control function Note

  • updates the active LED bit in ESL basic state register according to the actual status of all LEDs

Returns

  • sl_status_t


esl_led_get_count#

uint8_t esl_led_get_count ()

Get ESL Tag LED count Returns

  • Number of available LEDs


esl_led_is_srgb#

bool esl_led_is_srgb (uint8_t led_index)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aled_index

Get ESL Tag LED count Returns

  • Number of available LEDs


esl_core_respones_init#

void esl_core_respones_init ()

Init ESL Tag responses queue. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.


esl_core_build_response#

sl_status_t esl_core_build_response (tlv_t tlv, const void * input_data)
Parameters
TypeDirectionArgument NameDescription
tlv_t[in]tlv

The TLV to create the response stream for

const void *[in]input_data

can be a pointer to the basic status, led status etc.

Create response byte stream for single TLV based on input data and error status (if any) then puts the response stream into a circular buffer. The resulting output length of a single TLV will be the length encoded in that particular TLV + 1 byte as per ESL specification. Multiple response streams will be then concatenated on consecutive calls up to the maximum length limit of 48 bytes for multiple response data. Note

  • the actual length of the input data length MUST be in correspondence with the TLV passed as the first parameter!

Returns

  • sl_tatus_t


esl_core_get_responses#

uint8_t esl_core_get_responses (uint8_t remaining_length, uint8_t * buf_p)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]remaining_length

size of data out buffer

uint8_t *[out]buf_p

pointer to data buffer to copy the responses into

Copy all possible responses from internal circular buffer to a temporary linear buffer. Circular buffer drops the successfully read out data, while it might keep remaining responses which doesn't fit into the target buffer. Consistency of any response will be kept, that is, it might copy less data than the allowed maximum length passed as the first parameter, if there are responses left still in the internal circular buffer which otherwise wont fit into the target buffer. Returns

  • overall length of responses, might be 0 if there's no response


esl_sensor_init#

void esl_sensor_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

ESL Tag sensor init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.


esl_sensor_read#

sl_status_t esl_sensor_read (uint8_t index)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

Read interface (only) for ESL Sensor. Returns

  • sl_status_t SL_NOT_SUPPORTED if the ESL Sensor component is missing.


esl_sensor_get_count#

uint8_t esl_sensor_get_count (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get ESL Tag Sensor count Returns

  • Number of available sensors


esl_display_create#

sl_status_t esl_display_create (uint16_t width, uint16_t height, esl_display_type_t type, esl_display_info_p * info)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]width

Display horizontal pixel count.

uint16_t[in]height

Display vertical pixel count.

esl_display_type_t[in]type

Display type defined in BT SIG Assigned Numbers.

esl_display_info_p *[out]info

esl_display_info_p type pointer to the newly created display info data. This value needs to pass to esl_display_add call, which has to follow the invocation of esl_display_create for any new display to be created, fully and properly.

Create an ESL Tag display. Any display which a Tag wants to implement needs to becreated properly in the first place.

Returns

  • sl_status_t


esl_display_add#

sl_status_t esl_display_add (esl_display_info_p info, esl_va_method_p init_func, esl_va_method_p write_func)
Parameters
TypeDirectionArgument NameDescription
esl_display_info_p[in]info

esl_display_info_p type pointer, can be get by calling esl_display_create previously.

esl_va_method_p[in]init_func

esl_va_method_p type pointer to the low-level init function of the display driver. Driver implementation, however, it's up to the user to implement it properly - the only rule is to follow the interface specification defined by the esl_va_method_p type. If the 'init' method is not necessary for the given display, then a NULL pointer can be passed.

esl_va_method_p[in]write_func

esl_va_method_p type pointer to the low-level write function of the display driver. Has to be implemented by the users, and it's mandatory (can't be NULL).

Add an ESL Tag display to the list of available displays after creation. Any display on a Tag can be only used after adding it to the list.

Returns

  • sl_status_t


esl_display_bt_on_event#

void esl_display_bt_on_event (sl_bt_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_bt_msg_t *[in]evt

Event coming from the Bluetooth stack.

ESL display's bluetooth stack event handler. This one runs by the user implementation (usually in app.c) in parallel.


esl_display_set_image#

sl_status_t esl_display_set_image (uint8_t display_index, uint8_t image_index)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]display_index

Selects the display to show the image on.

uint8_t[in]image_index

Selects the image to be shown on the display.

ESL Display: chose an image to show. Invokes the users write_func passed to esl_display_add as its 3rd parameter. Returns

  • sl_status_t


esl_display_get_width#

sl_status_t esl_display_get_width (uint8_t display_index, uint16_t * width)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]display_index

Selects the display to get the width of.

uint16_t *[out]width

Horizontal pixel count of the selected display.

Display width getter. Returns

  • sl_status_t


esl_display_get_height#

sl_status_t esl_display_get_height (uint8_t display_index, uint16_t * height)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]display_index

Selects the display to get the height of.

uint16_t *[out]height

Vertical pixel count of the selected display.

Display height getter Returns

  • sl_status_t


esl_display_get_type#

sl_status_t esl_display_get_type (uint8_t display_index, esl_display_type_t * type)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]display_index

Selects the display to get the type of.

esl_display_type_t *[out]type

esl_display_type_t Display type defined in BT SIG.

Display type getter. Returns

  • sl_status_t


esl_led_add#

sl_status_t esl_led_add (esl_led_type_t type, uint8_t red_value, uint8_t green_value, uint8_t blue_value)
Parameters
TypeDirectionArgument NameDescription
esl_led_type_t[in]type

Possible ESL LED type defined by ESL standard

uint8_t[in]red_value

ESL LED (initial, in case of sRGB type) red color value.

uint8_t[in]green_value

ESL LED (initial, if sRGB) green color value.

uint8_t[in]blue_value

ESL LED (initial, if sRGB) blue color value.

Add an ESL Tag LED to the list of available LEDs after creation. Any LED on a Tag can be only used after adding it to the internal LED registry.

Returns

  • sl_status_t


esl_led_on#

sl_status_t esl_led_on (uint8_t led_index, esl_led_gamut_control_t gamut)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aled_index
esl_led_gamut_control_tN/Agamut

ESL Tag LED on function. Simple turn on function with given brightness and color values, to be implemented by end users. It's the users responsibility to actually turn given LED on with the given brightness and color parameters (if applicable) and the function shall return SL_STATUS_OK in case of success. Return SL_STATUS_FAIL on any other case (e.g. index out of bound, detectable HW error etc. Returns

  • sl_status_t


esl_led_off#

sl_status_t esl_led_off (uint8_t led_index)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aled_index

ESL Tag LED off function. Simple turn off function, similar to sl_esl_led_on method except it omits the gamut parameter entirely. To be implemented by end users. It's the users responsibility to actually turn given LED off and the function shall return SL_STATUS_OK in case of success. Return SL_STATUS_FAIL on any other case (e.g. index out of bound, detectable HW error etc. Returns

  • sl_status_t


esl_led_create_color#

esl_led_gamut_control_t esl_led_create_color (uint8_t red_value, uint8_t green_value, uint8_t blue_value, uint8_t brightness)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]red_value

ESL LED red color level

uint8_t[in]green_value

ESL LED red color level

uint8_t[in]blue_value

ESL LED red color level

uint8_t[in]brightness

ESL LED red color level

Assembly ESL Tag LED gamut value from input parameters for esl_led_gamut_control_t type Returns

  • esl_led_gamut_control_t Resulting ESL LED gamut value


esl_led_bt_on_event#

void esl_led_bt_on_event (sl_bt_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_bt_msg_t *[in]evt

Event coming from the Bluetooth stack.

ESL LED's bluetooth stack event handler. This one runs by the user implementation (usually in app.c) in parallel.


Macro Definition Documentation#

ESL_TAG_ADVERTISING_INTERVAL_MIN#

#define ESL_TAG_ADVERTISING_INTERVAL_MIN
Value:
750

ESL_TAG_ADVERTISING_INTERVAL_MAX#

#define ESL_TAG_ADVERTISING_INTERVAL_MAX
Value:
1500

ESL_TAG_MAX_SYNC_LOST_COUNT#

#define ESL_TAG_MAX_SYNC_LOST_COUNT
Value:
3

ESL_TAG_VENDOR_OPCODES_ENABLED#

#define ESL_TAG_VENDOR_OPCODES_ENABLED
Value:
1

ESL_TAG_BUILTIN_BATTERY_MEASURE_ENABLE#

#define ESL_TAG_BUILTIN_BATTERY_MEASURE_ENABLE
Value:
1

ESL_TAG_BATTERY_LEVEL_FULL_MILLIVOLTS#

#define ESL_TAG_BATTERY_LEVEL_FULL_MILLIVOLTS
Value:
3200

ESL_TAG_BATTERY_LEVEL_LOW_MILLIVOLTS#

#define ESL_TAG_BATTERY_LEVEL_LOW_MILLIVOLTS
Value:
2400

ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MIN#

#define ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MIN
Value:
10

ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MS#

#define ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MS
Value:
  (ESL_TAG_BATTERY_MEASUREMENT_INTERVAL_MIN * 60 * 1000)

ESL_TAG_BATTERY_LEVEL_UNKNOWN#

#define ESL_TAG_BATTERY_LEVEL_UNKNOWN
Value:
0

Definition for unknown battery voltage level (an implausible value)


ESL_DISPLAY_TYPE_BLACK_WHITE#

#define ESL_DISPLAY_TYPE_BLACK_WHITE
Value:
0x01

ESL Display Type Assigned Numbers.


ESL_DISPLAY_TYPE_3_GRAY_SCALE#

#define ESL_DISPLAY_TYPE_3_GRAY_SCALE
Value:
0x02

ESL_DISPLAY_TYPE_4_GRAY_SCALE#

#define ESL_DISPLAY_TYPE_4_GRAY_SCALE
Value:
0x03

ESL_DISPLAY_TYPE_8_GRAY_SCALE#

#define ESL_DISPLAY_TYPE_8_GRAY_SCALE
Value:
0x04

ESL_DISPLAY_TYPE_16_GRAY_SCALE#

#define ESL_DISPLAY_TYPE_16_GRAY_SCALE
Value:
0x05

ESL_DISPLAY_TYPE_RED_BLACK_WHITE#

#define ESL_DISPLAY_TYPE_RED_BLACK_WHITE
Value:
0x06

ESL_DISPLAY_TYPE_YELLOW_BLACK_WHITE#

#define ESL_DISPLAY_TYPE_YELLOW_BLACK_WHITE
Value:
0x07

ESL_DISPLAY_TYPE_RED_YELLOW_BLACK_WHITE#

#define ESL_DISPLAY_TYPE_RED_YELLOW_BLACK_WHITE
Value:
0x08

ESL_DISPLAY_TYPE_7_COLOR#

#define ESL_DISPLAY_TYPE_7_COLOR
Value:
0x09

ESL_DISPLAY_TYPE_16_COLOR#

#define ESL_DISPLAY_TYPE_16_COLOR
Value:
0x0A

ESL_DISPLAY_TYPE_FULL_RGB#

#define ESL_DISPLAY_TYPE_FULL_RGB
Value:
0x0B

ESL_ERROR_UNSPECIFIED#

#define ESL_ERROR_UNSPECIFIED
Value:
((esl_error_t)0x01)

Unspecified Error: any error condition that is not covered by a specific error code below


ESL_ERROR_INVALID_OPCODE#

#define ESL_ERROR_INVALID_OPCODE
Value:
((esl_error_t)0x02)

Invalid Opcode: The opcode was not recognized.


ESL_ERROR_INVALID_STATE#

#define ESL_ERROR_INVALID_STATE
Value:
((esl_error_t)0x03)

Invalid State: The request was not valid for the present ESL state.


ESL_ERROR_INVALID_IMAGE_INDEX#

#define ESL_ERROR_INVALID_IMAGE_INDEX
Value:
((esl_error_t)0x04)

Invalid Image Index: The Image_Index value was out of range.


ESL_ERROR_IMAGE_NOT_AVAILABLE#

#define ESL_ERROR_IMAGE_NOT_AVAILABLE
Value:
((esl_error_t)0x05)

Image Not Available: The requested image contained no image data.


ESL_ERROR_INVALID_PARAMETER#

#define ESL_ERROR_INVALID_PARAMETER
Value:
((esl_error_t)0x06)

Invalid Parameter(s): The parameter value(s) or length did not match the opcode


ESL_ERROR_CAPACITY_LIMIT#

#define ESL_ERROR_CAPACITY_LIMIT
Value:
((esl_error_t)0x07)

Capacity Limit: The required response could not be sent as it would exceed the payload size limit


ESL_ERROR_INSUFFICIENT_BATTERY#

#define ESL_ERROR_INSUFFICIENT_BATTERY
Value:
((esl_error_t)0x08)

Insufficient Battery: The request could not be processed because of a lack of battery charge


ESL_ERROR_INSUFFICIENT_RESOURCES#

#define ESL_ERROR_INSUFFICIENT_RESOURCES
Value:
((esl_error_t)0x09)

Insufficient Resources: The request could not be processed because of a lack of resources. This may be a temporary condition.


ESL_ERROR_RETRY#

#define ESL_ERROR_RETRY
Value:
((esl_error_t)0x0A)

Retry: The ESL is temporarily not able to give a full response (e.g., because the required sensor hardware was asleep) and the AP is asked to try the same command again.


ESL_ERROR_QUEUE_FULL#

#define ESL_ERROR_QUEUE_FULL
Value:
((esl_error_t)0x0B)

Queue Full: The ESL is temporarily unable to add a further timed command to the queue of pending commands ­the queue has reached its limit.


ESL_ERROR_IMPLAUSIBLE_TIME#

#define ESL_ERROR_IMPLAUSIBLE_TIME
Value:
((esl_error_t)0x0C)

Implausible time: The Absolute Time parameter value in the command would result in a delay longer than 48 days (that is, it's a possible overflow)


ESL_ERROR_VENDOR_NOERROR#

#define ESL_ERROR_VENDOR_NOERROR
Value:
((esl_error_t)0xFF)

No Error: 0xFF is reserved for 'no error' indication. For internal use only, and it is Silicon Labs specific.


ESL_ERROR_VENDOR_NOREPORT#

#define ESL_ERROR_VENDOR_NOREPORT
Value:
((esl_error_t)0xFE)

No report: 0xFE is reserved for 'no error report needed for timed commands' indication. For internal use only, and it is Silicon Labs specific.


esl_core_clear_last_error#

#define esl_core_clear_last_error
Value:
()

Wrapper around esl_core_set_last_error() to clear the last error


esl_core_has_no_error#

#define esl_core_has_no_error
Value:
()

Wrapper around esl_core_get_last_error() to check if there's no error


ESL_IMAGE_OBJECT_BASE#

#define ESL_IMAGE_OBJECT_BASE
Value:
0x100u

ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.


ESL_LED_TYPE_SHIFT#

#define ESL_LED_TYPE_SHIFT
Value:
((esl_led_type_t)6)

ESL_LED_BRIGHTNESS_SHIFT#

#define ESL_LED_BRIGHTNESS_SHIFT
Value:
((esl_led_gamut_control_t)6)

ESL_LED_RED_GAMUT_SHIFT#

#define ESL_LED_RED_GAMUT_SHIFT
Value:
((esl_led_gamut_control_t)0)

ESL_LED_GREEN_GAMUT_SHIFT#

#define ESL_LED_GREEN_GAMUT_SHIFT
Value:
((esl_led_gamut_control_t)2)

ESL_LED_BLUE_GAMUT_SHIFT#

#define ESL_LED_BLUE_GAMUT_SHIFT
Value:
((esl_led_gamut_control_t)4)

ESL_LED_REPEATS_TYPE_MASK#

#define ESL_LED_REPEATS_TYPE_MASK
Value:
((esl_led_repeats_type_t)0x0001)

ESL_LED_REPEATS_TYPE_COUNT#

#define ESL_LED_REPEATS_TYPE_COUNT
Value:
((esl_led_repeats_type_t)0x0000)

ESL_LED_REPEATS_TYPE_TIME#

#define ESL_LED_REPEATS_TYPE_TIME
Value:
((esl_led_repeats_type_t)0x0001)

ESL_LED_REPEATS_DURATION_SHIFT#

#define ESL_LED_REPEATS_DURATION_SHIFT
Value:
((esl_led_repeats_type_t)0x0001)

ESL_LED_TYPE_SRGB#

#define ESL_LED_TYPE_SRGB
Value:
((esl_led_type_t)(0x00 << ESL_LED_TYPE_SHIFT))

ESL LED type definition: sRGB.


ESL_LED_TYPE_MONOCHROME#

#define ESL_LED_TYPE_MONOCHROME
Value:
((esl_led_type_t)(0x01 << ESL_LED_TYPE_SHIFT))

ESL LED type definition: Monochrome.


ESL_LED_TYPE_MASK#

#define ESL_LED_TYPE_MASK
Value:
((esl_led_type_t)0xC0)

ESL_LED_GENERIC_2BIT_MASK#

#define ESL_LED_GENERIC_2BIT_MASK
Value:
((esl_led_type_t)0x03)

ESL_LED_LEVEL_0#

#define ESL_LED_LEVEL_0
Value:
(0x00)

ESL LED color gamut / brightness values.


ESL_LED_LEVEL_1#

#define ESL_LED_LEVEL_1
Value:
(0x01)

ESL_LED_LEVEL_2#

#define ESL_LED_LEVEL_2
Value:
(0x02)

ESL_LED_LEVEL_3#

#define ESL_LED_LEVEL_3
Value:
(0x03)

ESL_LED_LEVEL_STEP_PERCENTAGE#

#define ESL_LED_LEVEL_STEP_PERCENTAGE
Value:
25

ESL LED color gamut / brightness step percentage.


esl_led_get_brightness#

#define esl_led_get_brightness
Value:
(esl_led_gamut_control_t) \
((_gamut & (ESL_LED_GENERIC_2BIT_MASK << ESL_LED_BRIGHTNESS_SHIFT)) \
>> ESL_LED_BRIGHTNESS_SHIFT)

Function like macro getter for 2-bit brightness value from a gamut value Returns

  • esl_led_gamut_control_t brightness


esl_led_get_red_value#

#define esl_led_get_red_value
Value:
(esl_led_gamut_control_t) \
((_gamut & (ESL_LED_GENERIC_2BIT_MASK << ESL_LED_RED_GAMUT_SHIFT)) \
>> ESL_LED_RED_GAMUT_SHIFT)

Function like macro getter for 2-bit red value from a gamut value Returns

  • esl_led_gamut_control_t red value


esl_led_get_green_value#

#define esl_led_get_green_value
Value:
(esl_led_gamut_control_t) \
((_gamut & (ESL_LED_GENERIC_2BIT_MASK << ESL_LED_GREEN_GAMUT_SHIFT)) \
>> ESL_LED_GREEN_GAMUT_SHIFT)

Function like macro getter for 2-bit green value from a gamut value Returns

  • esl_led_gamut_control_t green value


esl_led_get_blue_value#

#define esl_led_get_blue_value
Value:
(esl_led_gamut_control_t) \
((_gamut & (ESL_LED_GENERIC_2BIT_MASK << ESL_LED_BLUE_GAMUT_SHIFT)) \
>> ESL_LED_BLUE_GAMUT_SHIFT)

Function like macro getter for 2-bit blue value from a gamut value Returns

  • esl_led_gamut_control_t blue value


ESL_TLV_RESPONSE_ERROR#

#define ESL_TLV_RESPONSE_ERROR
Value:
((tlv_t)0x00)

The command could not be processed successfully.


ESL_TLV_RESPONSE_LED_STATE#

#define ESL_TLV_RESPONSE_LED_STATE
Value:
((tlv_t)0x01)

Acknowledgment of a request to control an LED.


ESL_TLV_RESPONSE_BASIC_STATE#

#define ESL_TLV_RESPONSE_BASIC_STATE
Value:
((tlv_t)0x10)

General acknowledgment containing ESL status data.


ESL_TLV_RESPONSE_DISPLAY_STATE#

#define ESL_TLV_RESPONSE_DISPLAY_STATE
Value:
((tlv_t)0x11)

Acknowledgment of a request to display an image.


ESL_TLV_RESPONSE_SENSOR_VALUE#

#define ESL_TLV_RESPONSE_SENSOR_VALUE
Value:
((tlv_t)0x0E)

Sensor report.


ESL_TLV_RESPONSE_VENDOR_VALUE#

#define ESL_TLV_RESPONSE_VENDOR_VALUE
Value:
((tlv_t)0x0F)

Response data as specified by the vendor of the ESL.


ESL_TLV_TAG_MASK#

#define ESL_TLV_TAG_MASK
Value:
((tlv_t)0x0F)

Mask for getting the Tag value from an ESL TLV.


ESL_TLV_LEN_MASK#

#define ESL_TLV_LEN_MASK
Value:
((tlv_t)0xF0)

Mask for getting the Length value from an ESL TLV.


esl_core_get_tlv_tag#

#define esl_core_get_tlv_tag
Value:
(tlv_byte)

Function like macro getter for 'Tag' field from an ESL TLV Returns

  • tlv_tag_t 'Tag' value of the TLV


esl_core_get_tlv_len#

#define esl_core_get_tlv_len
Value:
((tlv_t) \
((tlv_byte & ESL_TLV_LEN_MASK) >> 4) + 1)

Function like macro getter for real 'Length' value from an ESL TLV Returns

  • tlv_length_t 'Length' value of the TLV


esl_core_set_tlv_tag#

#define esl_core_set_tlv_tag
Value:
do { \
_tlv &= (tlv_t)(~ESL_TLV_TAG_MASK); \
_tlv |= (((tlv_t)(_tag)) \
& ESL_TLV_TAG_MASK); \
} while (0)

Function like macro for setting the 'Tag' value of a TLV


esl_core_set_tlv_len#

#define esl_core_set_tlv_len
Value:
do { \
_tlv &= (tlv_t)(~ESL_TLV_LEN_MASK); \
_tlv |= _tlv | (((tlv_t)(((_len) - 1) << 4)) \
& ESL_TLV_LEN_MASK); \
} while (0)

Function like macro for setting the 'Length' value of a TLV


ESL_DISPLAY_INIT_FUNC_PARAMETERS_COUNT#

#define ESL_DISPLAY_INIT_FUNC_PARAMETERS_COUNT
Value:
(1)

ESL Display extra parameters count for init_func esl_va_method function.


ESL_DISPLAY_WRITE_FUNC_PARAMETERS_COUNT#

#define ESL_DISPLAY_WRITE_FUNC_PARAMETERS_COUNT
Value:
(2)

ESL Display extra parameters count for write_func esl_va_method function.