Air Quality GATT Service#
Provides air quality sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.
Functions#
void
sl_gatt_service_gas_on_event(sl_bt_msg_t *evt)
sl_status_t
sl_gatt_service_gas_get(uint16_t *eco2, uint16_t *tvoc)
Function Documentation#
sl_gatt_service_gas_on_event#
void sl_gatt_service_gas_on_event (sl_bt_msg_t *evt)
Parameters
[in] | evt | Event coming from the Bluetooth stack. |
Bluetooth stack event handler.
Definition at line
45
of file common/gatt_service_gas/sl_gatt_service_gas.h
sl_gatt_service_gas_get#
sl_status_t sl_gatt_service_gas_get (uint16_t *eco2, uint16_t *tvoc)
Parameters
[out] | eco2 | Equivalent CO2 level (in ppm). |
[out] | tvoc | Total Volatile Organic Compounds level (in ppb). |
Getter for ECO2 and TVOC characteristic values. Returns
Status of the operation.
Note
To be implemented in user code.
Definition at line
54
of file common/gatt_service_gas/sl_gatt_service_gas.h
Macro Definition Documentation#
SL_GATT_SERVICE_GAS_ECO2_INVALID#
#define SL_GATT_SERVICE_GAS_ECO2_INVALIDValue:
0xFFFF
Definition at line
43
of file common/gatt_service_gas/config/sl_gatt_service_gas_config.h
SL_GATT_SERVICE_GAS_TVOC_INVALID#
#define SL_GATT_SERVICE_GAS_TVOC_INVALIDValue:
0xFFFF
Definition at line
47
of file common/gatt_service_gas/config/sl_gatt_service_gas_config.h