Filter Accept List#

Filter Accept List.

Provides support for adding and removing devices from the Filter Accept List in the Bluetooth controller.

The Filter Accept List allows filtering transmissions from other Bluetooth devices so that the local device only receives/accepts transmissions from the devices that it's interested in or wants to communicate with. Operations that support filtering provide a means to control how the Filter Accept List is used:

Functions#

sl_status_t
sl_status_t
sl_bt_accept_list_add_device_by_address(bd_addr address, uint8_t address_type)
sl_status_t
sl_status_t
sl_bt_accept_list_remove_device_by_address(bd_addr address, uint8_t address_type)

Function Documentation#

sl_bt_accept_list_add_device_by_bonding#

sl_status_t sl_bt_accept_list_add_device_by_bonding (uint32_t bonding)
Parameters
[in]bonding

The bonding handle

Add a device to the Filter Accept List based on its bonding handle.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 12090 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_add_device_by_address#

sl_status_t sl_bt_accept_list_add_device_by_address (bd_addr address, uint8_t address_type)
Parameters
[in]address

Bluetooth address of the peer device

[in]address_type

Enum sl_bt_gap_address_type_t. The peer device address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_anonymous_address (0xff): Anonymous address. A Filter Accept List entry with this type matches all advertisements sent with no address.

Add a device to the Filter Accept List based on its identity address.

Use the special address type sl_bt_gap_anonymous_address to add an entry that matches all advertisements sent with no address.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 12111 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_remove_device_by_bonding#

sl_status_t sl_bt_accept_list_remove_device_by_bonding (uint32_t bonding)
Parameters
[in]bonding

The bonding handle

Remove a device from the Filter Accept List based on its bonding handle.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 12123 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_remove_device_by_address#

sl_status_t sl_bt_accept_list_remove_device_by_address (bd_addr address, uint8_t address_type)
Parameters
[in]address

Bluetooth address of the peer device

[in]address_type

Enum sl_bt_gap_address_type_t. The peer device address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_anonymous_address (0xff): Anonymous address. A Filter Accept List entry with this type matches all advertisements sent with no address.

Remove a device from the Filter Accept List based on its identity address.

Use the special address type sl_bt_gap_anonymous_address to remove an entry that matches all advertisements sent with no address.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 12144 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_remove_all_devices#

sl_status_t sl_bt_accept_list_remove_all_devices ()

Remove all devices from the Filter Accept List.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 12155 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_cmd_accept_list_add_device_by_bonding_id#

#define sl_bt_cmd_accept_list_add_device_by_bonding_id
Value:
0x005e0020

Definition at line 12070 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_accept_list_add_device_by_address_id#

#define sl_bt_cmd_accept_list_add_device_by_address_id
Value:
0x015e0020

Definition at line 12071 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_accept_list_remove_device_by_bonding_id#

#define sl_bt_cmd_accept_list_remove_device_by_bonding_id
Value:
0x025e0020

Definition at line 12072 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_accept_list_remove_device_by_address_id#

#define sl_bt_cmd_accept_list_remove_device_by_address_id
Value:
0x035e0020

Definition at line 12073 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_accept_list_remove_all_devices_id#

#define sl_bt_cmd_accept_list_remove_all_devices_id
Value:
0x045e0020

Definition at line 12074 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_accept_list_add_device_by_bonding_id#

#define sl_bt_rsp_accept_list_add_device_by_bonding_id
Value:
0x005e0020

Definition at line 12075 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_accept_list_add_device_by_address_id#

#define sl_bt_rsp_accept_list_add_device_by_address_id
Value:
0x015e0020

Definition at line 12076 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_accept_list_remove_device_by_bonding_id#

#define sl_bt_rsp_accept_list_remove_device_by_bonding_id
Value:
0x025e0020

Definition at line 12077 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_accept_list_remove_device_by_address_id#

#define sl_bt_rsp_accept_list_remove_device_by_address_id
Value:
0x035e0020

Definition at line 12078 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_accept_list_remove_all_devices_id#

#define sl_bt_rsp_accept_list_remove_all_devices_id
Value:
0x045e0020

Definition at line 12079 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h