Data structure of the descriptor event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_descriptor_s::connection
Connection handle
Definition at line
8091
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
descriptor#
uint16_t sl_bt_evt_gatt_descriptor_s::descriptor
GATT characteristic descriptor handle
Definition at line
8092
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
uuid#
uint8array sl_bt_evt_gatt_descriptor_s::uuid
Descriptor UUID in little endian format
Definition at line
8093
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h