Data structure of the procedure_completed event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_procedure_completed_s::connection
Connection handle
Definition at line
8193
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
result#
uint16_t sl_bt_evt_gatt_procedure_completed_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8194
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h