Data structure of the service event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_service_s::connection
Connection handle
Definition at line
8035
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
service#
uint32_t sl_bt_evt_gatt_service_s::service
GATT service handle
Definition at line
8036
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
uuid#
uint8array sl_bt_evt_gatt_service_s::uuid
Service UUID in little endian format
Definition at line
8037
of file /mnt/raid/workspaces/ws.fiuNlsfVk/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h