Data structure of the scan_report event.
Public Attribute Documentation#
packet_type#
uint8_t sl_bt_evt_scanner_scan_report_s::packet_type
Bits 0..2 : advertising packet type
000 : Connectable scannable undirected advertising
001 : Connectable undirected advertising
010 : Scannable undirected advertising
011 : Non-connectable non-scannable undirected advertising
100 : Scan Response. Note that this is received only if the device is in active scan mode.
Bits 3..4 : Reserved for future
Bits 5..6 : data completeness
00: Complete
01: Incomplete, more data to come in new events
10: Incomplete, data truncated, no more to come
Bit 7 : legacy or extended advertising
0: Legacy advertising PDUs used
1: Extended advertising PDUs used
address_type#
uint8_t sl_bt_evt_scanner_scan_report_s::address_type
Enum sl_bt_gap_address_type_t.
Advertiser address type.
If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:
0: Public address
1: Random address
255: No address provided (anonymous advertising)
If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:
sl_bt_gap_public_address (0x0): Public device address
sl_bt_gap_static_address (0x1): Static device address
sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address
sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address
sl_bt_gap_anonymous_address (0xff): No address provided (anonymous advertising)
sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)
sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)
bonding#
uint8_t sl_bt_evt_scanner_scan_report_s::bonding
Bonding handle if the remote advertising device has previously bonded with the local device. Values:
SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding
Other: Bonding handle
primary_phy#
uint8_t sl_bt_evt_scanner_scan_report_s::primary_phy
Enum sl_bt_gap_phy_t. The PHY on which advertising packets are transmitted on the primary advertising channel. Ignore this field if the report is for a legacy advertising PDU. Values:
sl_bt_gap_phy_1m (0x1): 1M PHY
sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)
secondary_phy#
uint8_t sl_bt_evt_scanner_scan_report_s::secondary_phy
Enum sl_bt_gap_phy_t. The PHY on which advertising packets are transmitted on the secondary advertising channel. Ignore this field if the report is for a legacy advertising PDU. Values:
sl_bt_gap_phy_1m (0x1): 1M PHY
sl_bt_gap_phy_2m (0x2): 2M PHY
sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)
tx_power#
int8_t sl_bt_evt_scanner_scan_report_s::tx_power
TX power value in the received packet header. Units: dBm
Valid value range: -127 to 126
Value 127: information unavailable
rssi#
int8_t sl_bt_evt_scanner_scan_report_s::rssi
Signal strength indicator (RSSI) in the last received packet. Units: dBm
Range: -127 to +20
channel#
uint8_t sl_bt_evt_scanner_scan_report_s::channel
The channel number on which the last packet was received
periodic_interval#
uint16_t sl_bt_evt_scanner_scan_report_s::periodic_interval
The periodic advertising interval. Value 0 indicates no periodic advertising. Otherwise,
Range: 0x06 to 0xFFFF
Unit: 1.25 ms
Time range: 7.5 ms to 81.92 s