Air Quality GATT Service#

Provides air quality sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.

Functions#

void
sl_status_t
sl_gatt_service_gas_get(uint16_t *eco2, uint16_t *tvoc)

Macros#

#define
SL_GATT_SERVICE_GAS_ECO2_INVALID 0xFFFF
#define
SL_GATT_SERVICE_GAS_TVOC_INVALID 0xFFFF

Function Documentation#

sl_gatt_service_gas_on_event#

void sl_gatt_service_gas_on_event (sl_bt_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_bt_msg_t *[in]evt

Event coming from the Bluetooth stack.

Bluetooth stack event handler.


sl_gatt_service_gas_get#

sl_status_t sl_gatt_service_gas_get (uint16_t * eco2, uint16_t * tvoc)
Parameters
TypeDirectionArgument NameDescription
uint16_t *[out]eco2

Equivalent CO2 level (in ppm).

uint16_t *[out]tvoc

Total Volatile Organic Compounds level (in ppb).

Getter for ECO2 and TVOC characteristic values. Returns

  • Status of the operation.

Note

  • To be implemented in user code.