Data structure of the data_request event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_external_bondingdb_data_request_s::connection
Connection handle
11695
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
type#
uint8_t sl_bt_evt_external_bondingdb_data_request_s::type
Enum sl_bt_external_bondingdb_data_t. The requested bonding data type. Values:
sl_bt_external_bondingdb_data_remote_address (0x0): Identity address of the remote device, which a resolvable random address can be resolved to
sl_bt_external_bondingdb_data_remote_address_type (0x1): Type of the remote device identity address. Value 0 is public device address and 1 is static device address
sl_bt_external_bondingdb_data_remote_ltk (0x2): Long Term Key (LTK) used as central device. The value of this type must be stored securely.
sl_bt_external_bondingdb_data_local_ltk (0x3): Long Term Key (LTK) used as peripheral device. The value of this type must be stored securely.
sl_bt_external_bondingdb_data_remote_central_inf (0x4): Identification info used as a central device
sl_bt_external_bondingdb_data_local_central_inf (0x5): Identification info used as a central device
sl_bt_external_bondingdb_data_irk (0x6): Identity Resolving Key (IRK) of the remote device that is used for resolving its RPA addresses when the device is in privacy mode. The value of this type must be stored securely.
sl_bt_external_bondingdb_data_meta (0x7): Metadata about the bonding
sl_bt_external_bondingdb_data_gatt_client_config (0x8): The remote GATT client characteristic configurations
sl_bt_external_bondingdb_data_gatt_client_features (0x9): The remote GATT client supported features
sl_bt_external_bondingdb_data_gatt_db_hash (0xa): Latest local GATT database hash value that the remote client has seen for GATT robust caching feature
11696
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h