Data structure of the descriptor_value event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_descriptor_value_s::connection
Connection handle
Definition at line
8159
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
descriptor#
uint16_t sl_bt_evt_gatt_descriptor_value_s::descriptor
GATT characteristic descriptor handle
Definition at line
8160
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
offset#
uint16_t sl_bt_evt_gatt_descriptor_value_s::offset
Value offset
Definition at line
8161
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
value#
uint8array sl_bt_evt_gatt_descriptor_value_s::value
Descriptor value
Definition at line
8162
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h