Data structure of the notification_tx_completed event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_server_notification_tx_completed_s::connection
Connection handle
Definition at line
9798
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
count#
uint8_t sl_bt_evt_gatt_server_notification_tx_completed_s::count
Number of notifications that have been transmitted
Definition at line
9799
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h