Data structure of the report event.
Public Attribute Documentation#
sync#
uint16_t sl_bt_evt_periodic_sync_report_s::sync
Periodic advertising synchronization handle
5643
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
tx_power#
int8_t sl_bt_evt_periodic_sync_report_s::tx_power
TX power value in the received packet header. Units: dBm
Valid value range: -127 to 126
Value 127: information unavailable
5644
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
rssi#
int8_t sl_bt_evt_periodic_sync_report_s::rssi
Signal strength indicator (RSSI) in the latest received packet. Units: dBm
Range: -127 to +20
5648
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
cte_type#
uint8_t sl_bt_evt_periodic_sync_report_s::cte_type
The CTE type
0x00: AoA CTE
0x01: AoD CTE with 1us slots
0x02: AoD CTE with 2us slots
0xFF: No CTE
5651
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
data_status#
uint8_t sl_bt_evt_periodic_sync_report_s::data_status
Data completeness:
0: Complete
1: Incomplete, more data to come in new events
2: Incomplete, data truncated, no more to come
5656
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
counter#
uint8_t sl_bt_evt_periodic_sync_report_s::counter
The sequence number of this sl_bt_evt_periodic_sync_report event as a monotonically increasing counter that wraps from 255 to 0. There is a single counter for this event type that starts from value 0 when the Bluetooth stack is started and is never reset while the stack is running. This counter can be used to detect if one or more sl_bt_evt_periodic_sync_report events have been created by the stack but dropped due to problems such as temporarily running out of resources before the event reached the application.
5662
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
data#
uint8array sl_bt_evt_periodic_sync_report_s::data
Periodic advertising data
5674
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h