sl_bt_evt_resource_status#
Indicates that the memory buffer usage has crossed a threshold.
Modules#
sl_bt_evt_resource_status_s
Macros#
#define
Identifier of the status event.
Typedef Documentation#
sl_bt_evt_resource_status_t#
typedef struct sl_bt_evt_resource_status_s sl_bt_evt_resource_status_t
Definition at line 1586
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_resource_status_id#
#define sl_bt_evt_resource_status_id
Value:0x005f00a0
Identifier of the status event.
Definition at line 1576
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h