sl_bt_evt_scanner_legacy_advertisement_report#
Reports an advertising data or scan response packet from an advertising device that uses legacy advertising PDUs.
This event is used to report advertisements only if the application includes the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component
Otherwise, the sl_bt_evt_scanner_scan_report event is used for maintaining the backwards compatibility.
Modules#
sl_bt_evt_scanner_legacy_advertisement_report_s
Typedefs#
Macros#
#define
Identifier of the legacy_advertisement_report event.
Typedef Documentation#
sl_bt_evt_scanner_legacy_advertisement_report_t#
typedef struct sl_bt_evt_scanner_legacy_advertisement_report_s sl_bt_evt_scanner_legacy_advertisement_report_t
Definition at line
3945
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_scanner_legacy_advertisement_report_id#
#define sl_bt_evt_scanner_legacy_advertisement_report_idValue:
0x000500a0
Identifier of the legacy_advertisement_report event.
Definition at line
3846
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h