Data structure of the data event.

Public Attributes#

uint16_t
int8_t
int8_t

Public Attribute Documentation#

sync#

uint16_t sl_bt_evt_sync_data_s::sync

Periodic advertising synchronization handle


tx_power#

int8_t sl_bt_evt_sync_data_s::tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable


rssi#

int8_t sl_bt_evt_sync_data_s::rssi

Signal strength indicator (RSSI) in the latest received packet. Units: dBm

  • Range: -127 to +20


data_status#

uint8_t sl_bt_evt_sync_data_s::data_status

Data completeness:

  • 0: Complete

  • 1: Incomplete, more data to come in new events

  • 2: Incomplete, data truncated, no more to come


data#

uint8array sl_bt_evt_sync_data_s::data

Periodic advertising data