Data structure of the dtm_completed event.

Public Attributes#

uint16_t

Public Attribute Documentation#

result#

uint16_t sl_bt_evt_test_dtm_completed_s::result

Command result


Definition at line 10405 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

number_of_packets#

uint16_t sl_bt_evt_test_dtm_completed_s::number_of_packets

Number of packets

Only valid for sl_bt_test_dtm_end command.


Definition at line 10406 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h