sl_bt_evt_user_message_to_host#
Used by the target application on a device to initiate communication and send a message to the NCP host.
Do not send event messages in the context of the user command handling.
Modules#
sl_bt_evt_user_message_to_host_s
Typedefs#
Macros#
#define
sl_bt_evt_user_message_to_host_id 0x00ff00a0
Identifier of the message_to_host event.
Typedef Documentation#
sl_bt_evt_user_message_to_host_t#
typedef struct sl_bt_evt_user_message_to_host_s sl_bt_evt_user_message_to_host_t
Definition at line
15308
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_user_message_to_host_id#
#define sl_bt_evt_user_message_to_host_idValue:
0x00ff00a0
Identifier of the message_to_host event.
Definition at line
15298
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h