Simple Communication Interface (UART)#
Component that provides simple communication interface using UART. This component is mainly used in NCP communication cases. This is a No-Code component if used together with NCP Interface or NCP Host Communication Interface components.
Modules#
Functions#
Macros#
Function Documentation#
sl_simple_com_init#
void sl_simple_com_init (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Simple Comm Init.
sl_simple_com_step#
void sl_simple_com_step (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Step function (used in CPC mode)
sl_simple_com_transmit#
void sl_simple_com_transmit (uint32_t len, const uint8_t * data)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | N/A | len | |
| const uint8_t * | N/A | data | 
Transmit function
sl_simple_com_transmit_cb#
void sl_simple_com_transmit_cb (sl_status_t status)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_status_t | N/A | status | 
Transmit completed callback
sl_simple_com_receive#
void sl_simple_com_receive (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Receive function (used in UART mode)
sl_simple_com_receive_cb#
void sl_simple_com_receive_cb (sl_status_t status, uint32_t len, uint8_t * data)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_status_t | N/A | status | |
| uint32_t | N/A | len | |
| uint8_t * | N/A | data | 
Receive completed callback
sl_simple_com_os_task_init#
void sl_simple_com_os_task_init (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
OS initialization function - if the OS is present
sl_simple_com_os_task_proceed#
void sl_simple_com_os_task_proceed (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Function to trigger the OS task to proceed - if the OS is present
sl_simple_com_robust_pack_data#
size_t sl_simple_com_robust_pack_data (uint8_t * packed_data_ptr, const uint8_t * data, uint16_t len)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t * | [out] | packed_data_ptr | pointer where the packed data should be loaded | 
| const uint8_t * | [in] | data | pointer to the data to be packed | 
| uint16_t | [in] | len | size of the data to be packed | 
Pack data between preamble byte and (if turned on) CRC checksum This function adds a 3 byte header containing preamble byte, payload length, CRC flag and CRC value to the header. If CRC is required an 8 bit CRC value will be calculated for the payload and added to the end of packet.
Returns
- the size of packed data 
sl_simple_com_robust_unpack_data#
sl_simple_com_robust_result_t sl_simple_com_robust_unpack_data (uint8_t * data, size_t len)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t * | [in] | data | pointer to the data to be unpacked | 
| size_t | [in] | len | size of the data to be unpacked | 
Unpack packets from byte stream looking for valid headers. This function searches valid headers and extracts payload after the header into destination buffer. Header is validated by 4 bit header CRC and payload can be also validated by optional CRC check.
Returns
- the result of the action