sl_bt_evt_system_hardware_error#

Indicates that a hardware-related error has occurred.

Modules#

sl_bt_evt_system_hardware_error_s

Macros#

#define

Identifier of the hardware_error event.

Typedef Documentation#

sl_bt_evt_system_hardware_error_t#

typedef struct sl_bt_evt_system_hardware_error_s sl_bt_evt_system_hardware_error_t

Definition at line 854 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_system_hardware_error_id#

#define sl_bt_evt_system_hardware_error_id
Value:
0x050100a0

Identifier of the hardware_error event.


Definition at line 844 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h