sl_bt_evt_connection_closed#

Indicates that a connection was either closed or that no connection was established from a high duty cycle directed advertising.

If the application includes the component bluetooth_feature_connection_statistics and the connection was successfully opened, the event sl_bt_evt_connection_statistics is automatically triggered just before the connection closed event to provide the application with the final statistic values of the connection.

Modules#

sl_bt_evt_connection_closed_s

Macros#

#define

Identifier of the closed event.

Typedef Documentation#

sl_bt_evt_connection_closed_t#

typedef struct sl_bt_evt_connection_closed_s sl_bt_evt_connection_closed_t

Definition at line 7068 of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_closed_id#

#define sl_bt_evt_connection_closed_id
Value:
0x010600a0

Identifier of the closed event.


Definition at line 7051 of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h