You are viewing documentation for version:
sl_bt_evt_dfu_boot_failure#
This event indicates that an error, which prevents the device from booting, has occurred in bootloader.
Modules#
sl_bt_evt_dfu_boot_failure_s
Macros#
#define
Identifier of the boot_failure event.
Typedef Documentation#
sl_bt_evt_dfu_boot_failure_t#
typedef struct sl_bt_evt_dfu_boot_failure_s sl_bt_evt_dfu_boot_failure_t
Definition at line 176
of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_dfu_boot_failure_id#
#define sl_bt_evt_dfu_boot_failure_id
Value:0x010000a0
Identifier of the boot_failure event.
Definition at line 166
of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h