Periodic Advertising Configuration Flags#
Defines configuration flags for periodic advertising.
Macros#
#define
Macro Definition Documentation#
SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER#
#define SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWERValue:
0x1
Include the TX power in advertising packets.
Definition at line
3431
of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING#
#define SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISINGValue:
0x2
Automatically start the extended advertising on the advertising set. The advertising will be started in non-connectable and non-scannable mode.
Definition at line
3435
of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h