Connection TX status flags#
Defines the connection TX status flags reported by sl_bt_resource_get_connection_tx_status.
Macros#
Macro Definition Documentation#
SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_PACKET_OVERFLOW#
#define SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_PACKET_OVERFLOWValue:
0x1
The number of TX packets queued on a connection has overflowed the packet_count
that was effective at the time the connection opened. The packet count is configured with command sl_bt_resource_enable_connection_tx_report and is valid for subsequent connections.
When this bit is set, the packet_count
returned by sl_bt_resource_get_connection_tx_status is correct, but data_len
excludes the data bytes in the packets that overflowed the configured packet count.
1555
of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_CORRUPT#
#define SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_CORRUPTValue:
0x2
Internal inconsistency has been detected in the connection TX bookkeeping. When this bit is set, the application should consider both packet_count
and data_len
returned by sl_bt_resource_get_connection_tx_status to be unreliable.
1565
of file /mnt/raid/workspaces/ws.CkeUHbuKC/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h