You are viewing documentation for version:
PDFData structure of the attribute_value event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_server_attribute_value_s::connection
Connection handle
attribute#
uint16_t sl_bt_evt_gatt_server_attribute_value_s::attribute
Attribute Handle
att_opcode#
uint8_t sl_bt_evt_gatt_server_attribute_value_s::att_opcode
Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.
offset#
uint16_t sl_bt_evt_gatt_server_attribute_value_s::offset
Value offset
value#
uint8array sl_bt_evt_gatt_server_attribute_value_s::value
Value