You are viewing documentation for version:
PDFData structure of the boot event.
Public Attribute Documentation#
major#
uint16_t sl_bt_evt_system_boot_s::major
Major release version
minor#
uint16_t sl_bt_evt_system_boot_s::minor
Minor release version
patch#
uint16_t sl_bt_evt_system_boot_s::patch
Patch release number
build#
uint16_t sl_bt_evt_system_boot_s::build
Build number
bootloader#
uint32_t sl_bt_evt_system_boot_s::bootloader
Unused. Ignore this field.
uint16_t sl_bt_evt_system_boot_s::hw
Hardware type: the major chip revision number in the most significant byte and the minor revision in the least significant byte
hash#
uint32_t sl_bt_evt_system_boot_s::hash
Version hash