General BGAPI User Commands#
Demonstrates the communication between an NCP host and NCP target using BGAPI user messages, responses and events. Can be used as a starting point for creating custom commands or for testing purposes.
Macro Definition Documentation#
USER_CMD_PERIODIC_ASYNC_ID#
#define USER_CMD_PERIODIC_ASYNC_IDValue:
0x01
Definition at line
39
of file common/ncp_user_cmd/ncp_user_cmd.h
USER_CMD_PERIODIC_ASYNC_STOP_ID#
#define USER_CMD_PERIODIC_ASYNC_STOP_IDValue:
0x02
Definition at line
40
of file common/ncp_user_cmd/ncp_user_cmd.h
USER_CMD_GET_BOARD_NAME_ID#
#define USER_CMD_GET_BOARD_NAME_IDValue:
0x03
Definition at line
41
of file common/ncp_user_cmd/ncp_user_cmd.h
USER_CMD_RESPONSE_ID#
#define USER_CMD_RESPONSE_IDValue:
0x04
Definition at line
42
of file common/ncp_user_cmd/ncp_user_cmd.h
USER_CMD_PERIODIC_SYNC_ID#
#define USER_CMD_PERIODIC_SYNC_IDValue:
0x05
Definition at line
43
of file common/ncp_user_cmd/ncp_user_cmd.h
USER_RSP_GET_BOARD_NAME_LEN#
#define USER_RSP_GET_BOARD_NAME_LENValue:
8
Definition at line
45
of file common/ncp_user_cmd/ncp_user_cmd.h