Air pressure sensor#
Air pressure sensor driver abstraction designed for Thunderboard.
Functions#
sl_status_t
sl_sensor_pressure_init(void)
void
sl_status_t
sl_sensor_pressure_get(float *pressure)
Function Documentation#
sl_sensor_pressure_init#
sl_status_t sl_sensor_pressure_init (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Initialize pressure sensor.
Note
With certain boards (e.g. 4166A), using this initialization function enables other sensors, because they're on the same enable pin. Please take that into account when using this function.
Returns
Status of the operation.
sl_sensor_pressure_deinit#
void sl_sensor_pressure_deinit (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Deinitialize pressure sensor.
Warnings
With certain boards (e.g. 4166A), using this deinitialization function disables other sensors, because they're on the same enable pin. Please use with caution.
sl_sensor_pressure_get#
sl_status_t sl_sensor_pressure_get (float * pressure)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float * | [out] | pressure | Barometric pressure (in millibars).  | 
Getter for pressure sensor measurement data. Returns
Status of the operation.