sl_bt_evt_connection_statistics#

Provides the connection statistic values when the application includes the component bluetooth_feature_connection_statistics.

When the component is included by the application, this event is automatically triggered to provide the final statistics for the connection just before the sl_bt_evt_connection_closed event indicates that a connection has been closed. This event is also triggered when the application has requested reading the statistics using the command sl_bt_connection_read_statistics.

Modules#

sl_bt_evt_connection_statistics_s

Macros#

#define

Identifier of the statistics event.

Typedef Documentation#

sl_bt_evt_connection_statistics_t#

typedef struct sl_bt_evt_connection_statistics_s sl_bt_evt_connection_statistics_t

Definition at line 6036 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_statistics_id#

#define sl_bt_evt_connection_statistics_id
Value:
0x0a0600a0

Identifier of the statistics event.


Definition at line 5974 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h